- Wed May 28, 2014 8:35 am
#171520
A few questions for those of you that have worked with these:
- I am trying to detect when a person is present in an 8' circle. This is for an outdoor sculpture. For various reasons I could get into if anyone cares, normal solutions like PIR and ultrasonic have disadvantages. Do you think using a MLX90614 (standard 90° FOV) mounted 4'-5' high and pointed down could detect someone on the edge of the circle? I.e. it would only see legs and feet. I do NOT need to know the temperature, and accuracy is not an issue - I only need the sensor to see a numerically significant difference from its own temperature. The issue is only a very small part of its FOV could have the person in it. This is also for outdoors year-round, so ambient temperatures and clothing types will change a lot.
- I'm curious, why would anyone *not* want the "gradient compensated" version? e.g. MLX90614-ACA. From the datasheet, it sounds like it's always useful:
- I am trying to detect when a person is present in an 8' circle. This is for an outdoor sculpture. For various reasons I could get into if anyone cares, normal solutions like PIR and ultrasonic have disadvantages. Do you think using a MLX90614 (standard 90° FOV) mounted 4'-5' high and pointed down could detect someone on the edge of the circle? I.e. it would only see legs and feet. I do NOT need to know the temperature, and accuracy is not an issue - I only need the sensor to see a numerically significant difference from its own temperature. The issue is only a very small part of its FOV could have the person in it. This is also for outdoors year-round, so ambient temperatures and clothing types will change a lot.
- I'm curious, why would anyone *not* want the "gradient compensated" version? e.g. MLX90614-ACA. From the datasheet, it sounds like it's always useful:
"Melexis has introduced the xCx version of the MLX90614. In these MLX90614xCx, the thermal gradients are measured internally and the measured temperature is compensated for them. In this way, the MLX90614xCx is much less sensitive to thermal gradients induced from outside"Thanks all