tozian wrote:Mee_n_Mac wrote:The OP didn't say whether his/her Pi was an A (1.5W) or B (3.5W) model. I'd have estimated about a 1 W load from the case temp so it could be either a working A or a loafing B.
B! It's a B!
So let me repeat myself ...
I would agree that the 80C isn't too hot ... now. But I have to ask if the the Pi will be used outdoors (or indoors in an un-AC environment) and/or draw more current when doing more processing.
Right now, given a 55 - 60C rise over (an assumed) ambient temp and no heatsink, I'll say your B Pi is loafing about, not working hard and not consuming much power. I'd guess ~1W and a bit less (80%) in the 7805 and so that's about 200 - 250 mA current draw. But with more peripherals used and/or more processing, that draw could easily double or even triple. That means the power dissipated in the 7805 will also double or triple. And that means the 60C rise would need to be 120 or 180 C in order for that to happen. Your 7805 might survive a doubling but not a tripling in current drawn through it in it's present form.
Before you smoke it, add a (?better?) heatsink and/or some more convective cooling (a fan).