- Mon Feb 17, 2014 7:54 pm
#168577
I'm working on a design that has an LM2621 DC-DC Step-Up. The typical application circuit is below:
1, 500 Ohm resistor. How critical is that? I want to stick with either a 0402 or 0603 package and Mouser doesn't have any, and Digi-Key has one in the 1/20W range. So I'm wondering if I can substitute it for a slightly different value and if so, which way should I swing, down to 499 Ohm or up to 510 Ohm? Both of those are rather common at Mouser.
The same question for that RF2, 50K Ohm. Another that doesn't seem very popular ...
My question is specifically regarding that RThe same question for that RF2, 50K Ohm. Another that doesn't seem very popular ...
You do not have the required permissions to view the files attached to this post.