- Wed Nov 13, 2013 3:24 am
#165508
Hi everyone,
I need to detect the distance of a point in space and i was wondering if using a IR Sensor or a Sonar.
I need an accuracy of around 2mm (i read that IR are a bit nasty when it comes to precision ).
Here's an example of the detection:
Basically,giving the facing direction of the sensor,i need to know the distance between the sensor origin and the
point A in a straight line.
What should be better?
Thanks in advance.
I need to detect the distance of a point in space and i was wondering if using a IR Sensor or a Sonar.
I need an accuracy of around 2mm (i read that IR are a bit nasty when it comes to precision ).
Here's an example of the detection:
Basically,giving the facing direction of the sensor,i need to know the distance between the sensor origin and the
point A in a straight line.
What should be better?
Thanks in advance.