A quick Google search brought this up.
Code: Select all//
// This is a simple program for testing the STMicroelectrics 3-axis gyroscope sold by Parallax.
//
// If you are new to the sensor you'll find all you need here. Just rip out what you don't want to save RAM.
//
// If you are using an Arduino Uno R3 like me, connect the SCL line to pin A5. Connect the SDA line to pin A4.
// I don't know anything about the other boards. I'm new to Arduino.
//
// The sample code at Parallax is incorrect in a couple of places. This code follows the application notes from STM. In
// particular I want to note that I found it is very important to check status register 3 to make sure there is new
// data before trying to request it, or else you will get very noisy data.
//
// You can try modifying NUM_GYRO_SAMPLES and GYRO_SIGMA_MULTIPLE.
// These control the statistical averaging that is used to discard bad values.
// The NUM_GYRO_SAMPLES can be reduced for faster calibration, but accuracy will start to suffer if you go below 50 samples.
// Increase the GYRO_SIGMA_MULTIPLE if you have an application that doesn't need to keep track of small rotations.
// Reduce GYRO_SIGMA_MULTIPLE if small rotations are important and you don't mind more noise in the data.
//
// If you are trying to create a compass from the gyro data then use the heading array I added. I found it pretty useful.
// If you set the sensor on your desk and only rotate it in yaw it works great. Turn it upside down and it's a mess, naturally.
//
// If you are putting the sensor in a robot hoping for dead reckoning it might work, but it may be necessary to recalibrate once
// in awhile with the robot stationary. It depends on how long your robot will be driving around and also how bumpy the
// surface is.
//
// Note that if you do not call updateGyro() often enough then you will miss data. You can check for this by looking at
// the status register's 7th bit. If it's on you've missed some data. It's possible to set up an interrupt to catch it. If you
// miss data then the report from the sensor isn't going to work as well for you.
//
// Use share and enjoy this however you like!
//
// Jim Bourke 2/6/2013 (RCGroups.com)
//
#include <Wire.h>
#define CTRL_REG1 0x20
#define CTRL_REG2 0x21
#define CTRL_REG3 0x22
#define CTRL_REG4 0x23
#define CTRL_REG5 0x24
#define CTRL_REG6 0x25
int gyroI2CAddr=105;
int gyroRaw[3]; // raw sensor data, each axis, pretty useless really but here it is.
double gyroDPS[3]; // gyro degrees per second, each axis
float heading[3]={0.0f}; // heading[x], heading[y], heading [z]
int gyroZeroRate[3]; // Calibration data. Needed because the sensor does center at zero, but rather always reports a small amount of rotation on each axis.
int gyroThreshold[3]; // Raw rate change data less than the statistically derived threshold is discarded.
#define NUM_GYRO_SAMPLES 50 // As recommended in STMicro doc
#define GYRO_SIGMA_MULTIPLE 3 // As recommended
float dpsPerDigit=.00875f; // for conversion to degrees per second
void setup() {
Serial.begin(115200);
Wire.begin();
setupGyro();
calibrateGyro();
}
void loop() {
updateGyroValues();
updateHeadings();
//testCalibration();
printDPS();
Serial.print(" --> ");
printHeadings();
Serial.println();
}
void printDPS()
{
Serial.print("DPS X: ");
Serial.print(gyroDPS[0]);
Serial.print(" Y: ");
Serial.print(gyroDPS[1]);
Serial.print(" Z: ");
Serial.print(gyroDPS[2]);
}
void printHeadings()
{
Serial.print("Heading X: ");
Serial.print(heading[0]);
Serial.print(" Y: ");
Serial.print(heading[1]);
Serial.print(" Z: ");
Serial.print(heading[2]);
}
void updateHeadings()
{
float deltaT=getDeltaTMicros();
for (int j=0;j<3;j++)
heading[j] -= (gyroDPS[j]*deltaT)/1000000.0f;
}
// this simply returns the elapsed time since the last call.
unsigned long getDeltaTMicros()
{
static unsigned long lastTime=0;
unsigned long currentTime=micros();
unsigned long deltaT=currentTime-lastTime;
if (deltaT < 0.0)
deltaT=currentTime+(4294967295-lastTime);
lastTime=currentTime;
return deltaT;
}
// I called this from the loop function to see what the right values were for the calibration constants.
// If you are trying to reduce the amount of time needed for calibration just try not to go so low that consecutive
// calibration calls give you completely unrelated data. Some sensors are probably better than others.
void testCalibration()
{
calibrateGyro();
for (int j=0;j<3;j++)
{
Serial.print(gyroZeroRate[j]);
Serial.print(" ");
Serial.print(gyroThreshold[j]);
Serial.print(" ");
}
Serial.println();
return;
}
// The settings here will suffice unless you want to use the interrupt feature.
void setupGyro()
{
gyroWriteI2C(CTRL_REG1, 0x1F); // Turn on all axes, disable power down
gyroWriteI2C(CTRL_REG3, 0x08); // Enable control ready signal
setGyroSensitivity500();
delay(100);
}
// Call this at start up. It's critical that your device is completely stationary during calibration.
// The sensor needs recalibration after lots of movement, lots of idle time, temperature changes, etc, so try to work that in to your design.
void calibrateGyro()
{
long int gyroSums[3]={0};
long int gyroSigma[3]={0};
for (int i=0;i<NUM_GYRO_SAMPLES;i++)
{
updateGyroValues();
for (int j=0;j<3;j++)
{
gyroSums[j]+=gyroRaw[j];
gyroSigma[j]+=gyroRaw[j]*gyroRaw[j];
}
}
for (int j=0;j<3;j++)
{
int averageRate=gyroSums[j]/NUM_GYRO_SAMPLES;
// Per STM docs, we store the average of the samples for each axis and subtract them when we use the data.
gyroZeroRate[j]=averageRate;
// Per STM docs, we create a threshold for each axis based on the standard deviation of the samples times 3.
gyroThreshold[j]=sqrt((double(gyroSigma[j]) / NUM_GYRO_SAMPLES) - (averageRate * averageRate)) * GYRO_SIGMA_MULTIPLE;
}
}
void updateGyroValues() {
while (!(gyroReadI2C(0x27) & B00001000)){} // Without this line you will get bad data occasionally
//if (gyroReadI2C(0x27) & B01000000)
// Serial.println("Data missed! Consider using an interrupt");
int reg=0x28;
for (int j=0;j<3;j++)
{
gyroRaw[j]=(gyroReadI2C(reg) | (gyroReadI2C(reg+1)<<8));
reg+=2;
}
int deltaGyro[3];
for (int j=0;j<3;j++)
{
deltaGyro[j]=gyroRaw[j]-gyroZeroRate[j]; // Use the calibration data to modify the sensor value.
if (abs(deltaGyro[j]) < gyroThreshold[j])
deltaGyro[j]=0;
gyroDPS[j]= dpsPerDigit * deltaGyro[j]; // Multiply the sensor value by the sensitivity factor to get degrees per second.
}
}
void setGyroSensitivity250(void)
{
dpsPerDigit=.00875f;
gyroWriteI2C(CTRL_REG4, 0x80); // Set scale (250 deg/sec)
}
void setGyroSensitivity500(void)
{
dpsPerDigit=.0175f;
gyroWriteI2C(CTRL_REG4, 0x90); // Set scale (500 deg/sec)
}
void setGyroSensitivity2000(void)
{
dpsPerDigit=.07f;
gyroWriteI2C(CTRL_REG4,0xA0);
}
int gyroReadI2C (byte regAddr) {
Wire.beginTransmission(gyroI2CAddr);
Wire.write(regAddr);
Wire.endTransmission();
Wire.requestFrom(gyroI2CAddr, 1);
while(!Wire.available()) {};
return (Wire.read());
}
int gyroWriteI2C( byte regAddr, byte val){
Wire.beginTransmission(gyroI2CAddr);
Wire.write(regAddr);
Wire.write(val);
Wire.endTransmission();
}
Google, Google, Google, Google, Google.....
------------------------------------------------------------------------------------------------------------------------------------------------------------
//codlink
Available for circuit and PCB design, just PM me!