SparkFun Forums 

Where electronics enthusiasts find answers.

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!
By Belial88
#164443
I'd like a voltage display. I see a ton of them on sites like this and ebay like with 7-segment displays. LCd, 7 segment, I'm okay with any of it.

I would like to attach them to my Z87X-UD3H's voltage read points, just solder them on:
Image

I see lots of displays for sale, it looks like I could just buy one and it's all good to go, but there's a few problems I have:

1. I need one that has x.xx voltage. All the ones I find only read to xx.x voltage.
2. I need to use external power, it can't draw from what it's reading as that'd be really screwy since those volts are going to the CPU and VRIN.
3. Voltage range of 1v to 3v. If you want me to be more specific, than .1v-1v to 1.7v (the lower min the better but i could live with a min of 1.3) and another at 1.8v to 2.6v.
4. Blue text (red is acceptable). 7-segment or LCD Blue negative (or red) i believe is what I have in mind.

That's all. I've considered just buying a DMM and just ripping it apart but... yea, hopefully I can avoid that.

Specifically, i'd like to solder it to my CPU Vcore and CPU VRIN points. I know I've talked about reading software/mobo readings in a similiar mod, but this needs to be hardware level and thus I can't use an arduino for this (or I could, but either way the data needs to come from these voltage read points. only other choice would be reading from the back of the phases but that's basically same thing...).

Thanks. I'm hoping this is an easy answer and just a simple "yea buy this off ebay, this guy just isn't listing all the info but we know this is the right thing" or "buy X parts and put it together'.
Last edited by Belial88 on Fri Oct 18, 2013 2:00 am, edited 2 times in total.
By Belial88
#164521
Sorry. Voltage range would be 1v to 3v. I can be more specific if necessary. I plan to just mount them inside my pc (which has a window) right next to the coltage read points on the mobo. Id use the psu's 5v or 12v but I can use batteries too.
By Belial88
#164536
What other surplus electronics outlets? I dont see anything on adafruit or sparkfun.

I'd prefer something in blue (i could live with red). Either in 7-segment or blue/red lettering (i believe it's called red negative, or blue negative).
By Belial88
#164637
lyndon wrote:Here! $1.90, can't beat that price!
Yes, this is exactly what I am finding only, and what I referenced. Like I say in the title and OP, I need one with .01 resolution, not .1 (ie x.xx instead of xx.x). That voltmeter also has a useless range. I need ~1-2v at least (ideally 0-3v but I could buy 2 different ones or I can sacrifice and just get one with 1.4-1.6v and one at 2-3v).

It also needs to use external power, which I'm not sure that one can do. The red text on that 7-seg is fine, i'd prefer blue, there are blue ones like the one you linked.

This is specically for CPU Vcore and CPU Vrin on haswell, so I'm watching my cpu's true voltage at ~1.4-1.6v range (high overclock, extremely dangerous burn-out voltages) and VRIN ~2.5).
Did you search for "panel meter" with google? Lots and lots of hits.
No, I haven't, I didn't know what this thing is called. I just searched voltage display. But I have now searched 'panel meter' and found nothing that meets my classification.

I don't feel like I'm asking too much here, I mean I could always rip a $40 DMM apart and do it I think.
By Mee_n_Mac
#164883
ADC = analog to digital converter

Yes you'd have to add the analogRead(pin#) and mod the existing code to scale and display the ADC reading. Should be easy. IIRC SF had another 'serial display', almost exactly the same, that had code to put it in a "DVM" mode. You might see if they still sell it.

FWIW I saw a number of digital panel meters via Google, I didn't search hard for blue 4 digit ones. I did see this. Perhaps they make a blue one ?
http://www.ebay.com/itm/0-36-4-Digit-Di ... 1006640099
By Belial88
#164893
LOL. Man you are too awesome for words to describe.

http://www.ebay.com/itm/DC-Voltmeter-4- ... 5af5ec162b

Just going to get a quick confirm here that this is what I'm looking for:
.01 resolution (that is, goes to the X.XX spot, ie 1.52v, 1.51v).
0-2.6v range at least
Runs off it's own power instead of source's power
Blue Text
Refresh rate: about 300mS / times;
Measure Range: DC 0-3.300V
Display Color: Blue
Input Polarity: DC voltage;
Overload: 4 times range;
Input impedance: 100Kohm;
Display: 4 digit 0.36" LED Tube
Accuracy: 0.002V
Power Supply: DC7-28V;
Operating temperature: -40 ℃ -85 ℃
Dimensions: 40.5mm x 24mm x 17.5mm
Cutting Size: 37.5mm x 21mm
Anti-reverse protection, Overrange display 0
So AC range, check. Blue, check. Resolution, check. I'm not sure on the dedicated power supply thing though. I see power supply DC7-28v, so I hope I can just hook these up to the 12v rails on my computer's PSU? They only need to be on when PC is on, as it's measuring CPU voltage and CPU VRIN voltage.

On a side note, dat hot glue... I'm going to ask them if they can send it to me in pieces or without that part stuck on, because getting it out of that hot glue is gong to be really messy time with heat gun..

!!!
By Mee_n_Mac
#164895
Belial88 wrote:DC7-28v, so I hope I can just hook these up to the 12v rails on my computer's PSU? They only need to be on when PC is on, as it's measuring CPU voltage and CPU VRIN voltage.
That's the way I read it. 12v supply should work.
By Belial88
#164958
Ah, they won't send it unassembled. It's okay, but let me look around a bit first.

I assume the wiring is Measure -> (+) of measured thing, Voltage line to power, and then for black... you splice it into 2 lines and one goes to power,one goes to (-) of what you measure. And if you were to use the power of what you measure, you would juts go black/measure to (-)/(+) of what you were measuring and leave red off.

I found this, searching for '4 digit voltmeters' that have a minimum voltage of 0:
http://www.ebay.com/itm/DC-0-33V-Blue-0 ... 4d04cc891d
Image


Display Type: 0,36" LED digital tube, 4 digit
Power Supply: DC4,5 -30V
Refresh Rate: about 500mS / times
Range: 0-33V
Input Polarity: DC voltage
Overload Capacity: 4 times range
Input Impedance: 100Kohm
Accuracy: ±(0.3‰ + 1 digit)
LED Size: 30×14mm
Board size: 36.60 ×14.80mm
Operating Temperature: -10℃ - 65℃
LED Color: Blue
Wiring:

3% of 1.5v = .0045. Plus one digit so... .0046 accuracy? So that means it's slightly worse than the previously mentioned display, but 10x the range?