- Fri Sep 27, 2013 12:26 pm
#163932
I have a Philips soundbar, model number CSS2123B/F7, and it is great, but it is not without its faults. One of my biggest complaints, is that it is very difficult to tell if it is turned on because there is only a small light on top of the soundbar that turns on and if it is positioned above your eye level, you cannot see the light. Also, this model allows you to adjust volume, bass, and treble levels, but there is no way to tell what the level is. In other words, you just keep pressing the button on the remote and the levels increase/decrease, but it is very annoying because if someone changes it, I have to keep adjusting it until I get it where I want. It would be much more convenient to be able to know a number, so that I can always have the levels set to the same.
I am currently in college studying electrical engineering, and I have a basic knowledge of all of this, but I love projects. That being said, I have given this project some thought, and I have come up with an approach, I am not sure if this is very feasible though.
Use some kind IF receiver to receive the signals from the remote. Then use some SSD LEDs to display what the current level is, and increment/decrement the number depending on the signal received. I would also like an LED to light up when the soundbar is turned on.
What parts would I need? How difficult will this project be?
Thanks so much!!
I am currently in college studying electrical engineering, and I have a basic knowledge of all of this, but I love projects. That being said, I have given this project some thought, and I have come up with an approach, I am not sure if this is very feasible though.
Use some kind IF receiver to receive the signals from the remote. Then use some SSD LEDs to display what the current level is, and increment/decrement the number depending on the signal received. I would also like an LED to light up when the soundbar is turned on.
What parts would I need? How difficult will this project be?
Thanks so much!!