- Wed Sep 25, 2013 10:05 am
#163860
Hello all,
I just found and bought a serial 3.2" TFT LCD module with Touch Panel. Also it came with a micro SD card (All of test source code and images are in it)
I have checked most of the project codes. they look ok.
Now I made a simple touch screen project to show you. It is the simplest and easiest way to build a very nice user interface. I high recommend to use this module for your project or products.
I use Arduino Duemilanove to build this project, you can use any MCU to control it.
Below is my test project information:
MCU:
Arduino Duemilanove (you can find it any where)
JP serial 3.2"TFT LCD Module (It come with TFT LCD and Micro SD Card)
http://www.jianpingusa.com
http://www.jianpingusa.com/jp32tftlcd_video.asp
Micro SD card code:
http://youtu.be/IPzeLQiHip8
http://youtu.be/ULyrTEIJZHE
Thanks to Sparkfun team and all forume users.
Oldspring
I just found and bought a serial 3.2" TFT LCD module with Touch Panel. Also it came with a micro SD card (All of test source code and images are in it)
I have checked most of the project codes. they look ok.
Now I made a simple touch screen project to show you. It is the simplest and easiest way to build a very nice user interface. I high recommend to use this module for your project or products.
I use Arduino Duemilanove to build this project, you can use any MCU to control it.
Below is my test project information:
MCU:
Arduino Duemilanove (you can find it any where)
JP serial 3.2"TFT LCD Module (It come with TFT LCD and Micro SD Card)
http://www.jianpingusa.com
http://www.jianpingusa.com/jp32tftlcd_video.asp
Micro SD card code:
Code: Select all
Arduino code:
L@,65535
LC,45,150,1,31,65535,OldSpring Touch Panel.
LC,95,110,1,31,65535,project test.
ZD,8
T3,0
L@,59160
Ld,115,120,90,90,59160
Le,120,125,80,80,59160
Mi,125,130,spring
T2,1,18,10,40,40,face1s,facedn
T2,2,78,10,40,40,face2s,facedn
T2,3,138,10,40,40,face3s,facedn
T2,4,198,10,40,40,face4s,facedn
T2,5,258,10,40,40,face5s,facedn
T2,6,18,60,40,40,face6s,facedn
T2,7,78,60,40,40,face7s,facedn
T2,8,138,60,40,40,face8s,facedn
T2,9,258,60,40,40,face9s,facedn
T2,10,198,60,40,40,faceas,facedn
T2,11,18,110,40,40,facebs,facedn
T2,12,258,110,40,40,face1s,facedn
T4,1
end
Code: Select all
/*==============================================================
File........JP Serial 3.2" TFT color LCD display module
A Touch Spring Test code for Arduino
Purpose.....This test code for JP Serial 3.2" TFT color LCD display module
Software....Arduino 1.52
MCU.........Arduino Duemilanove
Auther......OldSpring
Website.....WWW.-------.com
Email.......oldsprings@yahoo.com
Started.....
Updated.....
Note: The module Rx <===> Tx of Arduino
The module Tx <===> Rx of Arduino
=================== Parameter =============================*/
byte Serial_Read;
void setup()
{
Serial.begin(9600);
Serial.setTimeout(50);
delay(1000);
OldSpring();
}
void delay_m() {
delay(200);
}
// ================== Touch Spring Function Test =======================
void OldSpring() {
Serial.write("ZO,spring"); // Run a preprogram file in MMC card
Serial.write(13); // end char
delay(2000);
}
//=========================== System Loop ==============================
void loop(){
if (Serial.available() > 0) {
Serial_Read = Serial.read();
switch (Serial_Read) {
case 128: //Button Index = 1 "1"
Serial.write("Mi,125,130,face1");
Serial.write(13);
delay_m();
break;
case 129: //Button Index = 2 "2"
Serial.write("Mi,125,130,face2");
Serial.write(13);
delay_m();
break;
case 130: //Button Index = 3 "3"
Serial.write("Mi,125,130,face3");
Serial.write(13);
delay_m();
break;
case 131: //Button Index = 4 "4"
Serial.write("Mi,125,130,face4");
Serial.write(13);
delay_m();
break;
case 132: //Button Index = 5 "5"
Serial.write("Mi,125,130,face5");
Serial.write(13);
delay_m();
break;
case 133: //Button Index = 6 '6"
Serial.write("Mi,125,130,face6");
Serial.write(13);
delay_m();
break;
case 134: //Button Index = 7 "7"
Serial.write("Mi,125,130,face7");
Serial.write(13);
delay_m();
break;
case 135: //Button Index = 8 "8"
Serial.write("Mi,125,130,face8");
Serial.write(13);
delay_m();
break;
case 136: //Button Index = 9 "9"
Serial.write("Mi,125,130,face9");
Serial.write(13);
delay_m();
break;
case 137: //Button Index = 10 "0"
Serial.write("Mi,125,130,facea");
Serial.write(13);
delay_m();
break;
case 138: //Button Index = 11 "-"
Serial.write("Mi,125,130,faceb");
Serial.write(13);
delay_m();
break;
case 139: //Button Index = 12 "*"
Serial.write("Mi,125,130,face1");
Serial.write(13);
delay_m();
break;
case 140: //Button Index = 14 "/"
Serial.write("Mi,125,130,face2");
Serial.write(13);
delay_m();
break;
case 141: //Button Index = 15 "="
Serial.write("Mi,125,130,facea");
Serial.write(13);
delay_m();
break;
}
}}
http://youtu.be/IPzeLQiHip8
http://youtu.be/ULyrTEIJZHE
Thanks to Sparkfun team and all forume users.
Oldspring