- Fri Sep 13, 2013 6:21 am
#163472
I am looking for your feedback on a POV Globe I want to build. This is me vocalizing the possibility of doing this and publicly working out the math.
I want to build a plastic ring that would run from north to south at 0 and 180 degrees. I wanted to use the new Adafruit NeoPixel Digital RGB LED Strip at 144 LEDs and is 39.37" long and secure it to the plastic ring which is roughly 12.5" in diameter. That means there is an LED for every 2.5 degrees, however I plan to shift the ring so that the the first LED is at 0.625 degrees on the 0 degree strip so that second LED in POV will be at 1.875 on the 180 degree strip. By incorporating an offset in the display of the second strip, I can create a matrix instead of interlaced so that the 180 degree strip is 1.25 degrees after the 0 degree strip.
I am automatically assuming that I am going to need to split the strip in half. If I am spinning the globe at 30 rev/s that means each strip needs to program 72 LED in 38.6 micro seconds, hold them for the same amount, and then turn them off in the same amount of time to have some resemblance of a steady picture. With a 800kbps data rate for the neopixel, I will be 2160micro seconds to just program them.
It isn't even close to being able to work. I really wanted to use the Neopixel strips for ease of construction. Is my math even right?
Thanks,
Frank
I want to build a plastic ring that would run from north to south at 0 and 180 degrees. I wanted to use the new Adafruit NeoPixel Digital RGB LED Strip at 144 LEDs and is 39.37" long and secure it to the plastic ring which is roughly 12.5" in diameter. That means there is an LED for every 2.5 degrees, however I plan to shift the ring so that the the first LED is at 0.625 degrees on the 0 degree strip so that second LED in POV will be at 1.875 on the 180 degree strip. By incorporating an offset in the display of the second strip, I can create a matrix instead of interlaced so that the 180 degree strip is 1.25 degrees after the 0 degree strip.
I am automatically assuming that I am going to need to split the strip in half. If I am spinning the globe at 30 rev/s that means each strip needs to program 72 LED in 38.6 micro seconds, hold them for the same amount, and then turn them off in the same amount of time to have some resemblance of a steady picture. With a 800kbps data rate for the neopixel, I will be 2160micro seconds to just program them.
It isn't even close to being able to work. I really wanted to use the Neopixel strips for ease of construction. Is my math even right?
Thanks,
Frank