Advanced Helmet

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!

Moderator: phalanx

Post Reply
CoolAid
Posts: 4
Joined: Fri Oct 06, 2017 2:34 pm

Advanced Helmet

Post by CoolAid » Fri Oct 06, 2017 2:42 pm

Hello I am a newbe and -
I want to create a helmet that looks like a sci-fi helmet (mass effect, titanfall, halo, etc.) and that;

**Want to make cool helmet, need help with having multiple camera feed output to multiple (or one) screen(s)**


* Protects my head (able to decrease force from impact by significant degree)

* Can filter the air I breath (does not need to be super extreme filter, just filter out general junk, the better the filter the more pleased I am, but if it becomes too bulky/expensive then it is unnecessary)(Optional/Most Likely)

* Has a HUD with my vitals on it. I would wear some sensors, such as HR monitor to have some cool biofeedback, maybe also include other information.(option)

* Maybe even have it be a digital display where there are cameras on the front and maybe back of the helmet that they are displayed on the interior screen, where I have voice commands set up for some different things.

* Have the helmet be as sound proof as possible and have microphones where my ears would be, then inside the helmet speakers, so that I can modify the noise around me to be how I want it to be.

I understand this would be rather difficult (at least including all of the bullets) and that it could even be a touch silly. Yet, I find this a rather intriguing pursuit and think it will help contribute to becoming a cyborg. Any tips would be greatly appreciated as I don't really know where to start for this. I can imagine a lot of the work might be done on an Arduino, but I simply don't know the feasibility of modifying noises of the world around you and having the cameras on the helmet.



So here's a little prioritization sheet I worked out, it is not exactly in order, and maybe you all have some suggestions on what might be more critical to design and functionality.

Prioritization

1. Functionality


a. Head protection

a1. Padding/Inertia dampener
a2. Sturdy/solid

b. Control of phone through bluetooth

b1. In helmet speakers
b2. In helmet microphone
b3. Voice control

c. Control of other systems such as screens

c1. Voice control of screens
c2. Screen modification
c3. Screen HUD and other functions (maybe GPS map, time, etc.)

d. Camera view

d1. Camera live to screen with little to no latency
d1a. 360 degree view compressed to 180 degree screen (maybe)
d2. Computer control of camera feed
d2a. Visuals, different HUDs

e. Sound modulation

e1. Sound cancelling
e2. Sound reproduction at low to no latency
e3. Sound modification
e3a. Changing pitch
e3b. Change decibel levels
e3c. Change relative level of external sounds

f. The HUD

f1. Display of vitals
f1a. Heart rate, oxygenation, etc. (Requires some monitor)
f2. Display of time and other running interests
f3. Display of current location on google maps/GPS system

g. Air Filtration

g1. Filtration of air, relatively high quality
g2. Seal on head or seal over mouth and nose or full body suit that connects to helmet

h. Extra Features

2. Style
a. Look good
b. Look like popular sci-fi media
c. Does not interfere with functionality and accents functionality



How should I do this? I am planning on using some old phone screens if I can for the screen part and multiple cameras. I plan on using a raspberry computing system (might need multiple) to modulate the output from the cameras. How could I make multiple camera outputs lay onto multiple screens that looks good at three to five inches from the eyes? Also, how can I make the raspberry pi control my phone and computer via voice, or at least change a screens properties?

Thanks

jremington
Support Volunteer
Posts: 2220
Joined: Fri Jun 15, 2007 9:41 pm
Location: Eugene, Or

Re: Advanced Helmet

Post by jremington » Sat Oct 07, 2017 10:18 am

2. Style
a. Look good
b. Look like popular sci-fi media
c. Does not interfere with functionality and accents functionality
Protective helmets I've seen that also filter the air make the user look like a space alien or Darth Vader. If that is "looking good", start there.
Image

CoolAid
Posts: 4
Joined: Fri Oct 06, 2017 2:34 pm

Re: Advanced Helmet

Post by CoolAid » Tue Oct 10, 2017 5:20 pm

Does anyone know to configure the screen and the camera and a raspberry pi together.

Anthony Fremont
Posts: 23
Joined: Fri Oct 12, 2007 6:25 am

Re: Advanced Helmet

Post by Anthony Fremont » Wed Oct 11, 2017 7:04 am

CoolAid wrote:Does anyone know to configure the screen and the camera and a raspberry pi together.
Have you seen this?
https://www.zetronix.com/50-virtual-vid ... gLkPfD_BwE


Sent from my Moto G (4) using Tapatalk

CoolAid
Posts: 4
Joined: Fri Oct 06, 2017 2:34 pm

Re: Advanced Helmet

Post by CoolAid » Wed Oct 11, 2017 3:31 pm

Antony Fremont would I be able to toggle the input cameras?

Anthony Fremont
Posts: 23
Joined: Fri Oct 12, 2007 6:25 am

Re: Advanced Helmet

Post by Anthony Fremont » Sun Oct 15, 2017 6:42 am

CoolAid wrote:Antony Fremont would I be able to toggle the input cameras?
Seems like you'd just need to find a video switching device of some kind. Some kind of CMOS analog switch or multiplexer, probably could use pin diodes if you wanted to select the desired stream.

Sent from my Moto G (4) using Tapatalk

CoolAid
Posts: 4
Joined: Fri Oct 06, 2017 2:34 pm

Re: Advanced Helmet

Post by CoolAid » Thu Oct 19, 2017 2:01 pm

If you want to help but don’t know how.

Help financially by donating at

https://fundrazr.com/campaigns/01I1Cb
This is a big project, an to complete it I need your help!

Post Reply