PIC18F Setting RTC

Find out how to setup your programmer's software and how to solve many common problems.

Moderator: phalanx

Post Reply
mreiter
Posts: 11
Joined: Thu Feb 09, 2017 11:05 pm

PIC18F Setting RTC

Post by mreiter » Fri Feb 10, 2017 9:41 pm

Hello,

I just recently made a post here regarding an issue that I previously had with my SSPIF bit not being set during I2C (resulting in an infinite loop on start-up). I've since resolved that issue, and am no longer hanging on the start of i2c, but am still having trouble actually setting/reading from the RTC registers.

Again, I've included my i2c code. What I find interesting is the behaviour I get from this line:

Code: Select all

btfss	SSPCON1, WCOL
under the i2c_common_start label. I initially put this in to test collisions, but I find that I am (usually) able to set my RTC properly when configured like this. If I remove this line, then the RTC that I read (And ultimately display) is riddled with question marks "?", like this "??h?? ??/??/??". I presume this is an error in setting the values.

Any insights would be appreciated. Thanks

-Matthew

(code below)

Code: Select all

#include <p18f4620.inc>
#include <lcd.inc>

errorlevel -302
errorlevel -305

;global labels

variable _waitknt=0

udata
regaddress res 1
databyte res 1
datachar res 1
tens_digit res 1
ones_digit res 1
convert_buffer res 1

global write_rtc,read_rtc,rtc_convert,i2c_common_setup
global regaddress, databyte, datachar, tens_digit, ones_digit, convert_buffer


;; I2C MACROS
;;
;; Sebastian K, commit 110219-2208
;; forked off PIC16 sample code
;; for PIC18F4620
;; relocatable labels

;I2C lowest layer macros;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;

i2c_common_check_ack macro err_address ;If bad ACK bit received, goto err_address
btfsc SSPCON2,ACKSTAT
goto err_address
endm

i2c_common_start macro
;input: none
;output: none
;desc: initiate start condition on the bus
bsf SSPCON2,SEN
;btfss	SSPCON1, WCOL
bsf PIR1, SSPIF
btfss PIR1, SSPIF
bra $-2
bcf PIR1, SSPIF ;clear SSPIF interrupt bit

endm

i2c_common_stop macro
;input: none
;output: none
;desc: initiate stop condition on the bus
bsf SSPCON2,PEN
btfsc SSPCON2,PEN
bra $-2
bcf PIR1, SSPIF
endm

i2c_common_repeatedstart macro
;input: none
;output: none
;desc: initiate repeated start on the bus. Usually used for
; changing direction of SDA without STOP event
bsf SSPCON2,RSEN
btfss PIR1, SSPIF
bra $-2

bcf PIR1, SSPIF ;clear SSPIF interrupt bit

endm

i2c_common_ack macro
;input: none
;output: none
;desc: send an acknowledge to slave device
bcf SSPCON2,ACKDT
bsf SSPCON2,ACKEN
btfsc SSPCON2,ACKEN
bra $-2
endm

i2c_common_nack macro
;input: none
;output: none
;desc: send an not acknowledge to slave device

bsf SSPCON2,ACKDT
bsf SSPCON2,ACKEN

_waitl#v(_waitknt)
btfsc SSPCON2,ACKEN
goto _waitl#v(_waitknt)
_waitknt set _waitknt+1
endm

i2c_common_write macro

;input: W
;output: to slave device
;desc: writes W to SSPBUF and send to slave device. Make sure
; transmit is finished before continuing

btfsc SSPSTAT, BF
bra $-2

movwf SSPBUF

btfss PIR1, SSPIF
bra $-2
bcf PIR1, SSPIF ;clear SSPIF interrupt bit

endm

i2c_common_read macro
;input: none
;output: W
;desc: reads data from slave and saves it in W.

bsf SSPCON2,RCEN ;Begin receiving byte from
btfss PIR1, SSPIF
bra $-2
bcf PIR1, SSPIF
movf SSPBUF,w
endm
;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;

code

i2c_common_setup
;input: none
;output: none
;desc: sets up I2C as master device with 100kHz baud rate

movlw b'10000000'
movwf SSPSTAT ;set I2C line leves, clear all flags.

movlw 24 ;100kHz baud rate: 10000000 osc / [4*100000] -1
movwf SSPADD ;RTC only supports 100kHz

movlw b'00101000' ;Config SSP for Master Mode I2C
movwf SSPCON1

bsf SSPCON1,SSPEN ;Enable SSP module


bcf PIR2, SSPIE ;don't cause an interrupt on SSPIF, please. We're just polling it.
bcf PIR1, SSPIF
bcf SSPSTAT, BF
i2c_common_stop ;Ensure the bus is free
return

;rtc Algorithms;;;;;;

write_rtc

;input: address of register in RTC
;output: none
;Desc: handles writing data to RTC
;Select the DS1307 on the bus, in WRITE mode
i2c_common_start

movlw 0xD0 ;DS1307 address | WRITE bit
i2c_common_write
i2c_common_check_ack WR_ERR1

;Write data to I2C bus (Register Address in RTC)
movf regaddress,w ;Set register pointer in RTC
i2c_common_write ;
i2c_common_check_ack WR_ERR2

;Write data to I2C bus (Data to be placed in RTC register)
movf databyte,w ;Write data to register in RTC
i2c_common_write
i2c_common_check_ack WR_ERR3

goto WR_END

WR_ERR1
nop
movlw b'00001101'
movwf LATA

goto WR_END
WR_ERR2
nop
movlw b'00001111'
movwf LATA
bsf LATE,0
goto WR_END
WR_ERR3
nop
movlw b'00001001'
movwf LATA
goto WR_END
WR_END
i2c_common_stop ;Release the I2C bus
return

;; ************************************************** READ RTC
read_rtc
;input: address of RTC
;output: DOUT or 0x75
;Desc: This reads from the selected address of the RTC
; and saves it into DOUT or address 0x75

;Select the DS1307 on the bus, in WRITE mode

i2c_common_start

movlw 0xD0 ;DS1307 address | WRITE bit
i2c_common_write ;
i2c_common_check_ack RD_ERR1

;Write data to I2C bus (Register Address in RTC)
movf regaddress,w ;Set register pointer in RTC
i2c_common_write ;
i2c_common_check_ack RD_ERR2

;Re-Select the DS1307 on the bus, in READ mode
i2c_common_repeatedstart
movlw 0xD1 ;DS1307 address | READ bit
i2c_common_write
i2c_common_check_ack RD_ERR3

;Read data from I2C bus (Contents of Register in RTC)
i2c_common_read
movwf datachar
i2c_common_nack ;Send acknowledgement of data reception


goto RD_END

RD_ERR1
nop
movlw b'00000011'
movwf LATA
goto RD_END
RD_ERR2
nop
movlw b'00000101'
movwf LATA
goto RD_END
RD_ERR3
nop
movlw b'00000111'
movwf LATA
goto RD_END
;Release the I2C bus
RD_END
i2c_common_stop
return

rtc_convert
;input: W
;output: tens_digit, ones_digit
;desc: This subroutine converts the binary number
; in W into a two digit ASCII number and place
; each digit into the corresponding registers
; dig10 or dig1

movwf convert_buffer ; B1 = HHHH LLLL
swapf convert_buffer,w ; W = LLLL HHHH
andlw 0x0f ; Mask upper four bits 0000 HHHH
addlw 0x30 ; convert to ASCII
movwf tens_digit ;saves into 10ths digit

movf convert_buffer,w
andlw 0x0f ; w = 0000 LLLL
addlw 0x30 ; convert to ASCII
movwf ones_digit ; saves into 1s digit
return

end

User avatar
phalanx
Non-SFE Guru
Posts: 1983
Joined: Sun Nov 30, 2003 8:57 am
Location: Candia, NH

Re: PIC18F Setting RTC

Post by phalanx » Sat Feb 11, 2017 6:58 pm

What tools do you have at your disposal to track down your issue (debugger, scope, logic analyzer, etc.)? I don't have this particular combination of ICs to breadboard and test your code on so what you really need to do is look at the I2C waveform you are generating and see what it is you're doing or missing.

My hunch is there is something suspect of the timing of all your different I2C events. Many times a flag bit can be set indicating something has occurred but the I2C module hasn't fully completed its 9th bit period which results in a collision when you attempt the next action.

-Bill

User avatar
phalanx
Non-SFE Guru
Posts: 1983
Joined: Sun Nov 30, 2003 8:57 am
Location: Candia, NH

Re: PIC18F Setting RTC

Post by phalanx » Sun Feb 12, 2017 6:42 pm

So what needed fixing?

-Bill

mreiter
Posts: 11
Joined: Thu Feb 09, 2017 11:05 pm

Re: PIC18F Setting RTC

Post by mreiter » Sun Feb 12, 2017 7:28 pm

Hello Bill

It seems that I was a bit careless on my setup, changed the SSPSTAT configuration to "10000000", and in general covered up my exposed pins (I was leaving them floating, and this was not something the I2C pins enjoyed very much).

Thanks for showing interest and helping me out on these last few posts. I really appreciate it :)

Post Reply