Sending sdFat library error codes to lcd.print instead of serial

For the discussion of Arduino related topics.

Moderator: phalanx

Post Reply
dgog71
Posts: 1
Joined: Mon Nov 19, 2018 10:33 am

Sending sdFat library error codes to lcd.print instead of serial

Post by dgog71 » Mon Nov 19, 2018 10:54 am

Hi, I am relatively new to arduino and only ever asked 4 questions on the arduino forum. I am moving to this forum hoping it can be more helpful and less bullyish. here goes....

I am using the sdFat library.
I have coded a datalogger using it. I am using a LCD as I wish to use it independently of a computer and do not wish to use the serial port . Can anyone help me on how to get the sd card error codes that are generated within the sdFat library that are sent to serial to print through lcd.print instead. I usually find an answer eventually but this one eludes me. I have so found that the sdFat.h file has text I am trying to display on the lcd.
How do I change this class to print to the LCD??

Code: Select all

void initErrorPrint(Print* pr) {
    if (cardErrorCode()) {
      pr->println(F("Can't access SD card. Do not reformat.")); /// THIS LINE HERE!!!
      if (cardErrorCode() == SD_CARD_ERROR_CMD0) {
        pr->println(F("No card, wrong chip select pin, or SPI problem?"));
      }
      errorPrint(pr);
    } else if (vol()->fatType() == 0) {
      pr->println(F("Invalid format, reformat SD."));
    } else if (!vwd()->isOpen()) {
      pr->println(F("Can't open root directory."));
    } else {
      pr->println(F("No error found."));
    }
  }
I've looked through the libraries and on google but can't find any clues. I hope I've given enough info.
thanks for any help..

Code: Select all

#include <SPI.h>
#include "SdFat.h"

#include <DS1302RTC.h>
#include <TimeLib.h>

#include <Wire.h>
#include <Adafruit_AM2315.h>

#include <Adafruit_Sensor.h>
#include <Adafruit_TSL2561_U.h>

#include <LiquidCrystal_I2C.h>


// SD chip select pin.  Be sure to disable any other SPI devices such as Enet.
const uint8_t chipSelect = SS;

const uint32_t SAMPLE_INTERVAL_MS = 1000;// sample time

// Log file base name.  Must be six characters or less.
#define FILE_BASE_NAME "Data"



//------------------------------------------------------------------------------
// define the Real Time Clock object
DS1302RTC RTC(5, 6, 7);// Set pins:  CE, IO,CLK
// define AM2315 temperature humidity sensor object
Adafruit_AM2315 am2315;
//define TSL2561 object
Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);

LiquidCrystal_I2C lcd(0x3F, 20, 4);
// File system object.
SdFat sd;
// Log file.
SdFile file;


// Optional connection for RTC module
#define DS1302_GND_PIN 33
#define DS1302_VCC_PIN 35



int period = 1000;//millis timer
unsigned long time_now = 0;


// Time in micros for next data record.
uint32_t logTime;

//==============================================================================
// User functions.  Edit writeHeader() and logData() for your requirements.
//double TIME_1 = 0;// interrupts
//double INTERVAL_1 = 100;

const uint8_t CHANNEL_COUNT = 4;

float dataAM2315[2];
boolean AM2315_OK;

int dataLux;

float data[CHANNEL_COUNT]={88.88,88.88,88.88,88.88};
String label[4]={"C  :","RH :","LUX:","CO2:"};


//------------------------------------------------------------------------------
// Error messages stored in flash.
#define error(msg) sd.errorHalt(F(msg))

//------------------------------------------------------------------------------
void setup() {
	
	Serial.begin(115200);
	lcd.begin();
  const uint8_t BASE_NAME_SIZE = sizeof(FILE_BASE_NAME) - 1;
  char fileName[13] = FILE_BASE_NAME "00.csv";
 
  
  // Wait for USB Serial 
  while (!Serial) {
    SysCall::yield();
  }
  delay(500);
  
  if(!tsl.begin()||!am2315.begin())
  {
	  lcd.clear();
	  lcd.setCursor (0,1);
	  lcd.print("Sensors Unplugged");
	  while(1);
  }
   configureSensor();
  
/*	if (! am2315.begin()) {
	lcd.clear();
	lcd.setCursor (0,1);
	lcd.print("AM2315 Failed");
	while (1);
}
  */
   if (RTC.haltRTC()) {
	   lcd.clear();
	   lcd.setCursor (0,0);
	   lcd.print("RTC Failed");
	   while(1);
   }
   if (!RTC.writeEN()) {
	   lcd.clear();
	   lcd.setCursor (0,0);
	   lcd.print("RTC Found");
	   delay(1000);
   }
	lcd.clear();
	//
	lcd  .print(F("Sample Interval:"));
	lcd.setCursor (0,1);
	lcd.print(SAMPLE_INTERVAL_MS);
	lcd.print(F(" ms"));
	delay(1500);
 /*while (!Serial.available()) {
    SysCall::yield();
 }*/
  
  
  
  // Initialize at the highest speed supported by the board that is
  // not over 50 MHz. Try a lower speed if SPI errors occur.
  if (!sd.begin(chipSelect, SD_SCK_MHZ(40))) {
    sd.initErrorHalt();
}
  // Find an unused file name.
  if (BASE_NAME_SIZE > 6) {
    error("FILE_BASE_NAME too long");
  }
  while (sd.exists(fileName)) {
    if (fileName[BASE_NAME_SIZE + 1] != '9') {
      fileName[BASE_NAME_SIZE + 1]++;
    } else if (fileName[BASE_NAME_SIZE] != '9') {
      fileName[BASE_NAME_SIZE + 1] = '0';
      fileName[BASE_NAME_SIZE]++;
    } else {
      error("Can't create file name");
    }
  }
  if (!file.open(fileName, O_CREAT | O_WRITE | O_EXCL)) {
    error("file.open");
  }
  // Read any Serial data.
  do {
    delay(10);
  } while (Serial.available() && Serial.read() >= 0);
	lcd.clear();
	lcd.setCursor (0,1);
  lcd.print(("Log File:"));
  lcd.print(fileName);
 
	writeHeader();  // Write data header.

  logTime = micros()/(1000UL*SAMPLE_INTERVAL_MS) + 1;   // Start on a multiple of the sample interval.
  logTime *= 1000UL*SAMPLE_INTERVAL_MS;  
 }
 
	 
//------------------------------------------------------------------------------
void loop() {
	
	sensors_event_t event;
	tsl.getEvent(&event);
 
	 
 
  
	if(millis() > time_now + period){
		displayData();
		time_now = millis();
		AM2315_OK=am2315.readTemperatureAndHumidity(dataAM2315[0],dataAM2315[1]);
		/* Display the results (light is measured in lux) */
		if (event.light)
		{
			dataLux=event.light;
		}
	}
	
  // Time for next record.
  logTime += 1000UL*SAMPLE_INTERVAL_MS;

  // Wait for log time.
  int32_t diff;
  do {
    diff = micros() - logTime;
  } while (diff < 0);

  // Check for data rate too high.
  if (diff > 10) {
    error("Missed data record");
	
  }

  logData();
  // Force data to SD and update the directory entry to avoid data loss.
  if (!file.sync() || file.getWriteError()) {
    error("write error");
  }

  if (Serial.available()) {
	  //digitalWrite(greenLEDpin, LOW);
	  
    // Close file and stop.
    file.close();
	
	lcd.setCursor(0,1);
    lcd.print(("*** File Closed ***"));
    SysCall::halt();
  }
  
}

// Write data header.
void writeHeader() {
	file.print(F("UNIX"));
	file.print(F(",DateTime"));
	file.print(F(",micros"));
	file.print(F(",Temp"));
	file.print(F(",Hum"));
	file.print(F(",Lux"));
	file.print(F(",Co2"));
	//for (uint8_t i = 0; i < CHANNEL_COUNT; i++) {
		//file.print(F(",adc"));
		//file.print(i, DEC);
	//}
	file.println();
}
//------------------------------------------------------------------------------

// Log a data record.
void logData() {
	
	// Read all channels to avoid SD write latency between readings.
	for (uint8_t i = 0; i < 2; i++) {
		data[i] = dataAM2315[i];
		data[2]= dataLux;
		data[3]= 10;
	}
	// Write data to file.  Start with log time in micros.
	displayTime();	
	tStamp();//logging time stamp
	file.write (",");
	file.print(logTime); //use for accurate log timing

	// Write ADC data to CSV record.
	for (uint8_t i = 0; i < CHANNEL_COUNT; i++) {
		file.write(',');
		file.print(data[i]);
	}
	file.println();
	//

}
//==============================================================================

void configureSensor(void)
{
	
	tsl.enableAutoRange(true);           //auto range
	tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      //fast resoloution
	
}

void tStamp() {               // prints Date time to file
	tmElements_t tm;
	RTC.read(tm);
	// log time
	file.print(RTC.get()); // seconds since 1/1/1970
	file.print(",");
	file.print('"');
	file.print((tmYearToCalendar(tm.Year)), DEC);
	file.print("/");
	file.print((tm.Month),DEC);
	file.print("/");
	file.print((tm.Day), DEC);
	file.print("  ");
	logFile2digits(tm.Hour);
	file.print(":");
	logFile2digits(tm.Minute);
	file.print(":");
	logFile2digits(tm.Second);
	file.print('"');
}
void displayTime() {            ////prints date time to LCD
	tmElements_t tm;
	RTC.read(tm);
	// log time
	lcd.setCursor(0,0);
	
	lcd.print((tmYearToCalendar(tm.Year)), DEC);
	lcd.print("/");
	print2digits(tm.Month);
	lcd.print("/");
	print2digits(tm.Day);
	lcd.print("  ");
	print2digits(tm.Hour);
	lcd.print(":");
	print2digits(tm.Minute);
	lcd.print(":");
	print2digits(tm.Second);
	
}
void logFile2digits(int number) {
	if (number >= 0 && number < 10)
	file.write('0');
	file.print(number);
}
void print2digits(int number) {
	if (number >= 0 && number < 10)
	lcd.print('0');
	lcd.print(number);
}
void displayData() {
	for (uint8_t i = 0; i < 2; i++) { //first two columns of data
		lcd.setCursor(0,i+2);
		lcd.print(label[i]);
		lcd.setCursor(1,2);
		lcd.print((char)223);
		lcd.setCursor(4,i+2);
		lcd.print(data[i]);
	}
	for (uint8_t i = 2; i < 4; i++) {//last two columns of data
		lcd.setCursor(11,i);
		lcd.print(label[i]);
		lcd.setCursor(15,i);
		lcd.print(data[i]);
	}
}


Post Reply