SparkFun Forums 

Where electronics enthusiasts find answers.

For the discussion of Arduino related topics.
By monkstownman
#199821
I have bought two Lilypad Simblee BLE boards and cables from Sparkfun.
Please see attached image.

I am trying to upload the sample Blink file to either without success.

Below is the verbose output.

I have tried many different combinations from the tools menu.

avrdude: Version 6.3, compiled on Jan 17 2017 at 11:00:16
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch

System wide configuration file is "/home/johncog/.arduino15/packages/arduino/tools/avrdude/6.3.0-arduino9/etc/avrdude.conf"
User configuration file is "/home/johncog/.avrduderc"

Using Port : /dev/ttyUSB0
Using Programmer : arduino
Overriding Baud Rate : 115200
AVR Part : ATmega328P
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PC2
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :

Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 20 4 0 no 1024 4 0 3600 3600 0xff 0xff
flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff
lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00

Programmer Type : Arduino
Description : Arduino
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
Hardware Version: 4238238
Firmware Version: 32542464.0
Topcard : Unknown
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
Vtarget : 0.0 V
Varef : 3060382.4 V
Oscillator : Off
SCK period : 0.1 us

avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: initialization failed, rc=-1
Double check connections and try again, or use -F to override
this check.


avrdude done. Thank you.

Problem uploading to board. See http://www.arduino.cc/en/Guide/Troubleshooting#upload for suggestions.
You do not have the required permissions to view the files attached to this post.