Serial Communication

For the discussion of Arduino related topics.

Moderator: phalanx

Post Reply
jake3991
Posts: 1
Joined: Wed Dec 20, 2017 9:33 pm

Serial Communication

Post by jake3991 » Wed Dec 20, 2017 9:39 pm

I'm trying to live stream ultrasonic data from my ardunio to my Mac laptop and hitting a bit of a roadblock. The data the python script recovers does not change even when I move the sensor. I have verified the sensor is functioning by the serial monitor with the ardunio running. Any idea on what I need to do here to get the updated output from the ardunio? The code is below.

Code: Select all

// defines pins numbers
const int trigPin = 7;
const int echoPin = 8;

// defines variables
long duration;
int distance;

void setup() {
pinMode(trigPin, OUTPUT); // Sets the trigPin as an Output
pinMode(echoPin, INPUT); // Sets the echoPin as an Input
Serial.begin(9600); // Starts the serial communication
delayMicroseconds(50);
}

void loop() {
// Clears the trigPin
digitalWrite(trigPin, LOW);
delayMicroseconds(2);

// Sets the trigPin on HIGH state for 10 micro seconds
digitalWrite(trigPin, HIGH);
delayMicroseconds(10);
digitalWrite(trigPin, LOW);

// Reads the echoPin, returns the sound wave travel time in microseconds
duration = pulseIn(echoPin, HIGH);

// Calculating the distance in CM
distance= duration*0.034/2;

// Prints the distance on the Serial Monitor in CM
Serial.println(distance);

}

Code: Select all

import numpy
import serial 
import time
import sys
import cv2
import pickle 

#set up the camera stuff
cap = cv2.VideoCapture(1)

#container for images
images=[]

#container for distances
distances=[]

#first frame number
frame_num=1

#setup the serial connection and pause to establish it
ser = serial.Serial('/dev/cu.usbmodem1421', 9600,timeout=1)
time.sleep(5)


while True:
	try:
		#grab and image
		ret,frame=cap.read()

		#grab the distance
		distance=ser.readline()

		#process the image to a gray and 1241,376
		gray=cv2.cvtColor(frame, cv2.COLOR_BGR2GRAY)
		gray_resized=cv2.resize(gray,(1241,376))

		cv2.imshow("FRAME",gray_resized)
		print(distance)

		images.append([frame_num,gray_resized])
		distances.append([frame_num,distance])

	except KeyboardInterrupt:
		#pickle.dump( images, open( "save.p", "wb" ) )
		#pickle.dump( distances, open( "save.p", "wb" ) )

		sys.exit()

Post Reply