2x Xbee Series 1 with 1x Uno and 1x Mega
Posted: Wed Dec 06, 2017 9:44 am
Hi guys. I'm very new to arduino and xbee series 1. the main objective of my project is to able to control the lighting system from point A to point B using Xbee to transmit and receive. Right now i'm able to control the lighting from Xbee_A 'COM' by typing '1' as LED ON and '2' as LED OFF to the xbee_B. Furthermore, i would like to improvise the system by transferring data of the temperature values from point B back to point A. But i'm clueless on how to do that. Even after researching for days, i have no idea at all.
Xbee_A connected to shielding(https://www.cooking-hacks.com/communica ... xb-bt-rfid) to Arduino UNO
-jumper wire of DIN to pin 4, and DOUT to pin3
Xbee_B connection to shielding(https://www.cooking-hacks.com/communica ... xb-bt-rfid) to Arduino Mega
no jumper connection
TX CODE
Xbee_A connected to shielding(https://www.cooking-hacks.com/communica ... xb-bt-rfid) to Arduino UNO
-jumper wire of DIN to pin 4, and DOUT to pin3
Xbee_B connection to shielding(https://www.cooking-hacks.com/communica ... xb-bt-rfid) to Arduino Mega
no jumper connection
TX CODE
Code: Select all
RX CODE
#include<SoftwareSerial.h>
SoftwareSerial xbee(2,3);
char word1="";
void setup() {
// put your setup code here, to run once:
Serial.begin(9600);
xbee.begin(9600);
}
void loop() {
// put your main code here, to run repeatedly:
if(Serial.available()>0)//if key in something in COM
{
word1=Serial.read();//words equal what ou type
xbee.println(word1);//xbee print out words
Serial.print(word1);//
}
word1="";
Code: Select all
Any kind soul able to help me out with this? I would really grateful if anyone can help me out.#include <dht.h>
#define DHT22_PIN A8
int LED=13;
char letter;
dht DHT; //DHT 22
float hum; //Stores humidity value
float temp; //Stores temperature value
void setup()
{
Serial.begin(9600);
pinMode(13,OUTPUT);
}
void loop(){
if(Serial.available()==0){
int chk = DHT.read22(DHT22_PIN);
hum = DHT.humidity;
temp= DHT.temperature;
Serial.print("Humidity: ");
Serial.print(hum);
Serial.print(" %, Temp: ");
Serial.print(temp);
Serial.println(" Celsius");
}
if(Serial.available() >0)
{
letter = Serial.read();
if(letter == '1')
{
//50% brightness manually from control station
digitalWrite(LED, HIGH);
}
if (letter=='2')
{
digitalWrite(LED,LOW);
}
}
}