SparkFun Forums 

Where electronics enthusiasts find answers.

For the discussion of Arduino related topics.
By sgt_johnny
#195757
Hi!

I have made my own pcb with a Atmega32u4 as processor. I used the bootloader from Sparkfun (Fio V3). I have a 3.3V power source, 8 Mhz Crystal and the USB-Port is wired just like on the Sparkfun Schematic.

I have "burned" the bootloader via SPI with an Arduino Uno - worked
I uploaded a few sketches to test the hardware via SPI (Upload using programmer) - worked, but it terrible slow!

What i can't do is using usb to upload. The Board is found in device mangaer as "Sparkfun Fio v3 (COM 15)". When power the board up, and then want to upload the skech, the board dissapers from the device manager.

In the IDE it just does:
Code: Select all
Sketch uses 20398 bytes (71%) of program storage space. Maximum is 28672 bytes.
Global variables use 497 bytes of dynamic memory.
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
A few times until a timeout occurs. The Board seems now "stuck", it don't does anything, it does not run any sketch and hitting reset will NOT do anything (neihter execute the programm nor reappear in the device manager).

I have to power down and power up again to fix this.

I tried to initiate Upload, then push reset down, and unpush just the moment it wants to upload, this does something, it starts something that looks like it trys to upload:
Code: Select all
Warning: Board breadboard:avr:atmega328bb doesn't define a 'build.board' preference. Auto-set to: AVR_ATMEGA328BB
Sketch uses 20398 bytes (71%) of program storage space. Maximum is 28672 bytes.
Global variables use 497 bytes of dynamic memory.
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, } => {}
PORTS {COM1, } / {COM1, COM9, } => {COM9, }
Found upload port: COM9
C:\Users\Jonathan\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino8/bin/avrdude -CC:\Users\Jonathan\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino8/etc/avrdude.conf -v -patmega32u4 -cavr109 -PCOM9 -b57600 -D -Uflash:w:C:\Users\Jonathan\AppData\Local\Temp\arduino_build_297980/DOGM_test.ino.hex:i 

avrdude: Version 6.3, compiled on Dec 16 2016 at 13:33:19
         Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
         Copyright (c) 2007-2014 Joerg Wunsch

         System wide configuration file is "C:\Users\Jonathan\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino8/etc/avrdude.conf"

         Using Port                    : COM9
         Using Programmer              : avr109
         Overriding Baud Rate          : 57600
         AVR Part                      : ATmega32U4
         Chip Erase delay              : 9000 us
         PAGEL                         : PD7
         BS2                           : PA0
         RESET disposition             : dedicated
         RETRY pulse                   : SCK
         serial program mode           : yes
         parallel program mode         : yes
         Timeout                       : 200
         StabDelay                     : 100
         CmdexeDelay                   : 25
         SyncLoops                     : 32
         ByteDelay                     : 0
         PollIndex                     : 3
         PollValue                     : 0x53
         Memory Detail                 :

                                  Block Poll               Page                       Polled
           Memory Type Mode Delay Size  Indx Paged  Size   Size #Pages MinW  MaxW   ReadBack
           ----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
           eeprom        65    20     4    0 no       1024    4      0  9000  9000 0x00 0x00
           flash         65     6   128    0 yes     32768  128    256  4500  4500 0x00 0x00
           lfuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
           hfuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
           efuse          0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
           lock           0     0     0    0 no          1    0      0  9000  9000 0x00 0x00
           calibration    0     0     0    0 no          1    0      0     0     0 0x00 0x00
           signature      0     0     0    0 no          3    0      0     0     0 0x00 0x00

         Programmer Type : butterfly
         Description     : Atmel AppNote AVR109 Boot Loader

Connecting to programmer: .avrdude: butterfly_recv(): programmer is not responding

avrdude: butterfly_recv(): programmer is not responding

But then it stops :cry: :cry: :cry:

Any idea how to fix this?


Regards,
Jonathan