- Sat Jun 03, 2017 2:42 pm
#195063
Hi,
I am new to Arduino and have zero background in electronics, so please show mercy.
I have recently bought the MicroSD Breakout With Level Shifter, which worked excellent with my Arduino Uno. I have tried to connect it to my new Arduino Micro 5V, and it doesn't work. I am running the sketchs from the SD examples provided with the software. They worked well with the Uno, but they don't work with the Micro. I checked the wiring, and then re-checked them and then re-re-re checked them. They are OK.
The code is simply the SDinfo code, with the chipSelect changed to 8. I attach it below.
The error I get is:
This is so frustrating! I Will appreciate your help!
I am new to Arduino and have zero background in electronics, so please show mercy.
I have recently bought the MicroSD Breakout With Level Shifter, which worked excellent with my Arduino Uno. I have tried to connect it to my new Arduino Micro 5V, and it doesn't work. I am running the sketchs from the SD examples provided with the software. They worked well with the Uno, but they don't work with the Micro. I checked the wiring, and then re-checked them and then re-re-re checked them. They are OK.
The code is simply the SDinfo code, with the chipSelect changed to 8. I attach it below.
The error I get is:
Initializing SD card...initialization failed. Things to check:The answer to all of the above is yes.
* is a card inserted?
* is your wiring correct?
* did you change the chipSelect pin to match your shield or module?
This is so frustrating! I Will appreciate your help!
Code: Select all
/*
SD card test
This example shows how use the utility libraries on which the'
SD library is based in order to get info about your SD card.
Very useful for testing a card when you're not sure whether its working or not.
The circuit:
* SD card attached to SPI bus as follows:
** MOSI - pin 11 on Arduino Uno/Duemilanove/Diecimila
** MISO - pin 12 on Arduino Uno/Duemilanove/Diecimila
** CLK - pin 13 on Arduino Uno/Duemilanove/Diecimila
** CS - depends on your SD card shield or module.
Pin 4 used here for consistency with other Arduino examples
created 28 Mar 2011
by Limor Fried
modified 9 Apr 2012
by Tom Igoe
*/
// include the SD library:
#include <SPI.h>
#include <SD.h>
// set up variables using the SD utility library functions:
Sd2Card card;
SdVolume volume;
SdFile root;
// change this to match your SD shield or module;
// Arduino Ethernet shield: pin 4
// Adafruit SD shields and modules: pin 10
// Sparkfun SD shield: pin 8
// MKRZero SD: SDCARD_SS_PIN
const int chipSelect = 8;
void setup() {
// Open serial communications and wait for port to open:
Serial.begin(9600);
while (!Serial) {
; // wait for serial port to connect. Needed for native USB port only
}
Serial.print("\nInitializing SD card...");
// we'll use the initialization code from the utility libraries
// since we're just testing if the card is working!
if (!card.init(SPI_HALF_SPEED, chipSelect)) {
Serial.println("initialization failed. Things to check:");
Serial.println("* is a card inserted?");
Serial.println("* is your wiring correct?");
Serial.println("* did you change the chipSelect pin to match your shield or module?");
return;
} else {
Serial.println("Wiring is correct and a card is present.");
}
// print the type of card
Serial.print("\nCard type: ");
switch (card.type()) {
case SD_CARD_TYPE_SD1:
Serial.println("SD1");
break;
case SD_CARD_TYPE_SD2:
Serial.println("SD2");
break;
case SD_CARD_TYPE_SDHC:
Serial.println("SDHC");
break;
default:
Serial.println("Unknown");
}
// Now we will try to open the 'volume'/'partition' - it should be FAT16 or FAT32
if (!volume.init(card)) {
Serial.println("Could not find FAT16/FAT32 partition.\nMake sure you've formatted the card");
return;
}
// print the type and size of the first FAT-type volume
uint32_t volumesize;
Serial.print("\nVolume type is FAT");
Serial.println(volume.fatType(), DEC);
Serial.println();
volumesize = volume.blocksPerCluster(); // clusters are collections of blocks
volumesize *= volume.clusterCount(); // we'll have a lot of clusters
volumesize *= 512; // SD card blocks are always 512 bytes
Serial.print("Volume size (bytes): ");
Serial.println(volumesize);
Serial.print("Volume size (Kbytes): ");
volumesize /= 1024;
Serial.println(volumesize);
Serial.print("Volume size (Mbytes): ");
volumesize /= 1024;
Serial.println(volumesize);
Serial.println("\nFiles found on the card (name, date and size in bytes): ");
root.openRoot(volume);
// list all files in the card with date and size
root.ls(LS_R | LS_DATE | LS_SIZE);
}
void loop(void) {
}