- Thu Apr 20, 2017 12:56 pm
#194455
Hi all. I am building a control for a freezer. I need to start the freezer at the specified temp and shut off when that is satisfied. (I have that) What I'm having trouble with is, I need to have the compressor stay off for 3 minutes before starting again. This is a single stage freezer getting down to -50 F. It gets above the specified temp before 3 minutes and causes the compressor to attempt to come on and lock up. What I need, I think, is a way to override the if statement reading the probe, so the loop will not run until the 3 minutes have elapsed, without stopping the display from reading the temp. Thanks for any help.
again thanks for any help, i've been trying to get this for a few weeks.
not sure how many variations of delay,while loops and "and" functions I'v tried
Code: Select all
right now everything works but no time delay#include <OneWire.h>
#include <DallasTemperature.h>
// Data wire is plugged into pin 2 on the Arduino
#define ONE_WIRE_BUS 3
#define ct 5
// Setup a oneWire instance to communicate with any OneWire devices
// (not just Maxim/Dallas temperature ICs)
OneWire oneWire(ONE_WIRE_BUS);
// Pass our oneWire reference to Dallas Temperature.
DallasTemperature sensors(&oneWire);
int offtime=1500;
void setup(void)
{ pinMode(ct, OUTPUT);
// start serial port
Serial.begin(9600);
Serial.println(" ColdTrap");
elapsedMillis elapsedTime; // used by elapsedmilis example
// Globally scoped - see comment above
unsigned long off = millis(); // used by millis() example...
unsigned int interval = 1000;
// Start up the library
sensors.begin();
}
void loop(void)
{ delay (offtime);
// call sensors.requestTemperatures() to issue a global temperature
// request to all devices on the bus
Serial.print(" ");
sensors.requestTemperatures(); // Send the command to get temperatures
Serial.println(" ");
Serial.print(" ");
Serial.print(sensors.getTempFByIndex(0)); // Why "byIndex"?
// You can have more than one IC on the same bus.
// 0 refers to the first IC on the wire
{
{ if(sensors.getTempFByIndex(0) >= -50)
digitalWrite (ct, HIGH);
else
digitalWrite (ct, LOW);
again thanks for any help, i've been trying to get this for a few weeks.
not sure how many variations of delay,while loops and "and" functions I'v tried