- Wed Mar 08, 2017 8:32 am
#193784
i want to make countdown clock with adjustable time and control some relays
and i want to use 2 displays seven segment and lcd 20*2
lcd is working fine but seven segment is flickering.
and i want to use 2 displays seven segment and lcd 20*2
lcd is working fine but seven segment is flickering.
Code: Select all
#include <LiquidCrystal.h>
#include <Bounce2.h>
#include "SevSeg.h"
#define BUTTON_PINs 9
#define LED_PIN 13
#define feedback 8
#define BUTTON_PINin 22
#define BUTTON_PINp 10
#define BUTTON_PINn 11
#define BUTTON_PINr 12
#define BUTTON_PINf 27
#define BUTTON_PINb 26
#define BUTTON_PIN60 25
#define BUTTON_PIN30 24
Bounce debouncers = Bounce();
Bounce debouncerp = Bounce();
Bounce debouncern = Bounce();
Bounce debouncerr = Bounce();
Bounce debouncerin = Bounce();
Bounce debouncerf = Bounce();
Bounce debouncerb = Bounce();
Bounce debouncer60 = Bounce();
Bounce debouncer30 = Bounce();
int S = 00; // count seconds
int M = 60; // count minutes
int H = 00; // count hours
int ledState = LOW;
int feedbackState = LOW;
//initialize the library with the numbers of the interface pins
LiquidCrystal lcd(2, 3, 4, 5, 6, 7); // pins connected to LCD
SevSeg sevseg;
void setup()
{
byte numDigits = 4;
byte digitPins[] = {34, 32, 30, 28};
byte segmentPins[] = {36, 38, 40, 42, 44, 46, 48,37};
bool resistorsOnSegments = false; // Use 'true' if on digit pins
byte hardwareConfig = COMMON_ANODE; // See README.md for options
sevseg.begin(hardwareConfig, numDigits, digitPins, segmentPins, resistorsOnSegments);
sevseg.setBrightness(500);
pinMode(50, OUTPUT);
pinMode(51, OUTPUT);
pinMode(52, OUTPUT);
// pinMode(50, OUTPUT);
lcd.begin(16, 2); //set up the LCD's number of columns and rows
Serial.begin(9600);
pinMode(BUTTON_PINs, INPUT_PULLUP);
pinMode(BUTTON_PINp, INPUT_PULLUP);
pinMode(BUTTON_PINn, INPUT_PULLUP);
pinMode(BUTTON_PINr, INPUT_PULLUP);
pinMode(BUTTON_PINin, INPUT_PULLUP);
pinMode(BUTTON_PINf, INPUT_PULLUP);
pinMode(BUTTON_PINb, INPUT_PULLUP);
pinMode(BUTTON_PIN60, INPUT_PULLUP);
pinMode(BUTTON_PIN30, INPUT_PULLUP);
// After setting up the button, setup the Bounce instance :
debouncers.attach(BUTTON_PINs);
debouncers.interval(0);
debouncerp.attach(BUTTON_PINp);
debouncerp.interval(0);
debouncern.attach(BUTTON_PINn);
debouncern.interval(0);
debouncerr.attach(BUTTON_PINr);
debouncerr.interval(0);
debouncerin.attach(BUTTON_PINin);
debouncerin.interval(0);
debouncerf.attach(BUTTON_PINf);
debouncerf.interval(0);
debouncerb.attach(BUTTON_PINb);
debouncerb.interval(0);
debouncer60.attach(BUTTON_PIN60);
debouncer60.interval(0);
debouncer30.attach(BUTTON_PIN30);
debouncer30.interval(0);
pinMode(LED_PIN, OUTPUT);
pinMode(feedback, OUTPUT);
digitalWrite(LED_PIN, ledState);
digitalWrite(feedback, feedbackState);
}
void loop()
{
lcd.setCursor(1, 0);
lcd.print (" ");
// lcd.setCursor(10,1);
//lcd.print(":");
lcd.setCursor(13, 1);
lcd.print(":");
debouncers .update();
debouncerp .update();
debouncern .update();
debouncerr .update();
debouncerin.update();
debouncerf .update();
debouncerb .update();
debouncer60.update();
debouncer30.update();
// Get the updated value :
int values = debouncers .read();
int valuep = debouncerp .read();
int valuen = debouncern .read();
int valuer = debouncerr .read();
int valuein = debouncerin.read();
int valuef = debouncerf .read();
int valueb = debouncerb .read();
int value60 = debouncer60.read();
int value30 = debouncer30.read();
if ( valuep == HIGH ) {
M = (M + 1);
// delay(250);
}
if ( valuen == HIGH ) {
M = (M - 1);
// delay(250);
}
if ( value60 == HIGH ) {
M =60;
}
if ( value30 == HIGH ) {
M =30;
}
if ( valuef == HIGH ) {
digitalWrite(51, LOW);
digitalWrite(52, LOW);
}
else if ( valueb == HIGH ) {
digitalWrite(51, HIGH);
digitalWrite(52,HIGH);
}
if ( debouncers.fell() ) {
// Toggle LED state :
ledState = !ledState;
digitalWrite(LED_PIN, ledState);
feedbackState = !feedbackState;
digitalWrite(feedback, feedbackState);
}
if ( feedbackState == HIGH && M >= 0 && S >= 0 )
{
lcd.setCursor(0, 1);
lcd.print("TIME LEFT:");
S--;
delay(1000);
}
else {
S;
lcd.setCursor(0, 1);
lcd.print(" READY ");
}
if (S < 0)
{
M--;
S = 59;
}
if (M < 0)
{
H--;
M = 00;
}
if (H < 0)
{
H = 00;
M = 00;
S = 00;
}
if (M > 9)
{
lcd.setCursor(11, 1);
lcd.print(M);
sevseg.setNumber(M);
sevseg.refreshDisplay();
}
else
{
lcd.setCursor(11, 1);
lcd.print("0");
lcd.setCursor(12, 1);
lcd.print(M);
sevseg.setNumber(M);
sevseg.refreshDisplay();
lcd.setCursor(13, 1);
lcd.print(":");
}
if (S > 9)
{
lcd.setCursor(14, 1);
lcd.print(S);
}
else
{
lcd.setCursor(14, 1);
lcd.print("0");
lcd.setCursor(15, 1);
lcd.print(S);
lcd.setCursor(16, 1);
lcd.print(" ");
}
if (H > 9)
{
//lcd.setCursor(8,1);
//lcd.print (H);
}
else
{
//lcd.setCursor(8,1);
// lcd.print("0");
// lcd.setCursor(9,1);
// lcd.print(H);
// lcd.setCursor(10,1);
//lcd.print(":");
}
if (M == 0 && S == 0) {
digitalWrite(50, HIGH);
}
else if (valuein == LOW) {
digitalWrite(50, HIGH);
}
else if (valuein == LOW) {
digitalWrite(50, HIGH);
}
else
{
digitalWrite(50, LOW);
}
if ( valuer == HIGH ) {
digitalWrite(50, LOW);
}
else
{digitalWrite(50, HIGH);
}
}