- Mon Feb 13, 2017 12:35 pm
#193405
Hello, I am having a really weird issue with ProMicro. The story is that I need to make a custom keypad, each button must do some action by working as a keyboard - it's a GUI control keyboard. It's very simple, just 7 buttons, all laid out on a soldering board and connected properly. No wires are touching, everything is good. The buttons are connected to different pins to keep it simple.
I made a sketch to read the buttons using the internal pull-up resistor with debouncing, and it works, well mostly. The issue rises when I press the middle and up buttons (I call them select and up) (and sometimes it happens with the bottom, or down, button). It appears as if the connections short-circuit and different buttons gets read, however it's not the case. When a select button is pressed, it gets registered as an up button, but the up button registers as normal. Sometimes select/middle button registers as down button...
It might be hard to understand, so here's a lowdown: some buttons get read as different ones, although no connections are touching.
I have made a video to explain it better: https://youtu.be/TbHCbelg3MI
And here's the sketch I'm uploading:
I made a sketch to read the buttons using the internal pull-up resistor with debouncing, and it works, well mostly. The issue rises when I press the middle and up buttons (I call them select and up) (and sometimes it happens with the bottom, or down, button). It appears as if the connections short-circuit and different buttons gets read, however it's not the case. When a select button is pressed, it gets registered as an up button, but the up button registers as normal. Sometimes select/middle button registers as down button...
It might be hard to understand, so here's a lowdown: some buttons get read as different ones, although no connections are touching.
I have made a video to explain it better: https://youtu.be/TbHCbelg3MI
And here's the sketch I'm uploading:
Code: Select all
I'm starting to think that I've got a defective unit, haven't tried with different Arduinos though.#include <Keyboard.h>
// define number of pins we'll use
// otherwise it causes funky behaviour
const int numOfPins = 7;
// define pins on ProMicro with
// different delays for each button
int btnPins[numOfPins][2] = {
{2, 2000}, // exit
{3, 2000}, // back
{4, 250}, // right
{5, 250}, // down
{6, 2000}, // enter
{7, 250}, // up
{8, 250} // left
};
int val = 0;
long lastDebounceTime = 0;
void setup() {
for (int i = 0; i < numOfPins; i++) {
pinMode(btnPins[i][0], INPUT_PULLUP);
}
}
void loop() {
for (int i = 0; i < numOfPins; i++) {
if ((millis() - lastDebounceTime) > btnPins[i][1]) {
val = digitalRead(btnPins[i][0]);
if (val == LOW) {
// Serial.println(btnPins[i][0]);
doAction(btnPins[i][0]);
lastDebounceTime = millis();
}
}
}
}
void doAction(int pin) {
if (pin == btnPins[0][0]) {
Serial.println("exit");
// Keyboard.print("exit ");
} else if (pin == btnPins[1][0]) {
Serial.println("back");
// Keyboard.print("back ");
} else if (pin == btnPins[2][0]) {
Serial.println("right");
// Keyboard.print("right ");
} else if (pin == btnPins[3][0]) {
Serial.println("down");
// Keyboard.print("down ");
} else if (pin == btnPins[4][0]) {
Serial.println("enter");
// Keyboard.print("enter ");
} else if (pin == btnPins[5][0]) {
Serial.println("up");
// Keyboard.print("up ");
} else if (pin == btnPins[6][0]) {
Serial.println("left");
// Keyboard.print("left ");
}
}