- Sat Jan 28, 2017 2:59 pm
#193140
I am having trouble initializing my 3 SPI devices, a micro sd card module, usb host shield and RA8875.
The connection is sd_cs 4, RA8875_cs 5 and usb_cs 10. Here is my setup function.
void setup()
{
Serial.begin(9600);
pinMode(10,OUTPUT);
digitalWrite(10, HIGH);
pinMode(5,OUTPUT);
digitalWrite(5, HIGH);
pinMode(4, OUTPUT);
digitalWrite(4, HIGH);
digitalWrite(5, LOW);
Serial.println("RA8875 start");
//RA8875 initialize
if (!tft.begin(RA8875_800x480)) {
Serial.println("RA8875 Not Found!");
while (1);
}
Serial.println("Found RA8875");
//sd card initialize
digitalWrite(4, LOW);
if (!SD.begin(4)) {
Serial.println("SD initialization failed!");
return;
}
Serial.println("SD initialization done.");
digitalWrite(4, HIGH);
//usb initialize
digitalWrite(10,LOW);
delay(20);
digitalWrite(10,HIGH);
#if !defined(__MIPSEL__)
while (!Serial); // Wait for serial port to connect - used on Leonardo, Teensy and other boards with built-in USB CDC serial connection
#endif
Serial.println("Start USB");
if (Usb.Init() == -1)
Serial.println("OSC did not start.");
else
Serial.println("USB ready!");
digitalWrite(10,HIGH);
delay( 200 );
}
the ra8875 and sd card are fine but the usb host have an output "OSC did not start''
I really need help please
The connection is sd_cs 4, RA8875_cs 5 and usb_cs 10. Here is my setup function.
void setup()
{
Serial.begin(9600);
pinMode(10,OUTPUT);
digitalWrite(10, HIGH);
pinMode(5,OUTPUT);
digitalWrite(5, HIGH);
pinMode(4, OUTPUT);
digitalWrite(4, HIGH);
digitalWrite(5, LOW);
Serial.println("RA8875 start");
//RA8875 initialize
if (!tft.begin(RA8875_800x480)) {
Serial.println("RA8875 Not Found!");
while (1);
}
Serial.println("Found RA8875");
//sd card initialize
digitalWrite(4, LOW);
if (!SD.begin(4)) {
Serial.println("SD initialization failed!");
return;
}
Serial.println("SD initialization done.");
digitalWrite(4, HIGH);
//usb initialize
digitalWrite(10,LOW);
delay(20);
digitalWrite(10,HIGH);
#if !defined(__MIPSEL__)
while (!Serial); // Wait for serial port to connect - used on Leonardo, Teensy and other boards with built-in USB CDC serial connection
#endif
Serial.println("Start USB");
if (Usb.Init() == -1)
Serial.println("OSC did not start.");
else
Serial.println("USB ready!");
digitalWrite(10,HIGH);
delay( 200 );
}
the ra8875 and sd card are fine but the usb host have an output "OSC did not start''
I really need help please