- Sun Oct 16, 2016 12:40 am
#192037
Hey Sparkfunners! I'm an Arduino newbie looking for help choosing the best components for my project and some general guidance.
I'm building a public art piece for my local library. It will be an interactive fiction terminal the player reveals by pressing a glowing button embedded within a book displayed on the library shelves. The button will open a terminal and keyboard bay below by rotating them 90° and revealing the hardware underneath. Players will then be met with a prompt and custom game which introduces them to IF and text adventures.
I have the module bays built, balanced, hardware installed, and an Arduino handy. I'm having difficulty selecting the exact components so I can get my hands dirty coding and move forward. I've been looking to meet these requirements throughout the design process:
1. Can the motor supply the torque to rotate the module? (I don't have a good way of measuring this, but it's definitely more than average hobby motors)
2. Is the motor a modest size? (can fit within a 6"x6"x6" space)
3. Is the motor less than or around $30?
4. Is the motor not crazy loud? (it's in a library after all. It will still be insulated by books, which should help.)
5. Is it easy to control? (I don't have the experience necessary here, but get the impression stepper motors are more complex over DC motors to control, for example)
6. Is it compatible with an Adafruit Motor Shield v2? (This isn't absolutely necessary, but there's quite a bit of documentation and existing examples for using this shield. It would go a LONG way helping me learn to write the code for it if there's great documentation and examples).
7. Can both motors be powered and run off one shield? (I'm looking to control the motors to rotate both module bays at the same time).
I'm currently looking to use a Sparkfun Standard Gearmotor 6RPM (3-12V). It has some excellent torque (Stall Torque: 613 oz-in), is within my price range, and DC motors seem like a decent fit. It seems like it would take approximately 2.5 seconds to rotate the 90 degrees, which I am more than happy with. I'm still lost in a few areas:
1. Is this motor a realistic fit?
2. How can I tell if the Adafruit motor shield can power two of them at once?
3. How do I calculate the type of wall wart to actually power them? (I intend to power them from an outlet nearby, since batteries would require constant monitoring.)
4. If the torque is adequate, can I connect the drive shaft directly to the pivot rod on the module? Is this wise? What is the name of the component I would use exactly?
Any advice would be greatly appreciated.
I'm building a public art piece for my local library. It will be an interactive fiction terminal the player reveals by pressing a glowing button embedded within a book displayed on the library shelves. The button will open a terminal and keyboard bay below by rotating them 90° and revealing the hardware underneath. Players will then be met with a prompt and custom game which introduces them to IF and text adventures.
I have the module bays built, balanced, hardware installed, and an Arduino handy. I'm having difficulty selecting the exact components so I can get my hands dirty coding and move forward. I've been looking to meet these requirements throughout the design process:
1. Can the motor supply the torque to rotate the module? (I don't have a good way of measuring this, but it's definitely more than average hobby motors)
2. Is the motor a modest size? (can fit within a 6"x6"x6" space)
3. Is the motor less than or around $30?
4. Is the motor not crazy loud? (it's in a library after all. It will still be insulated by books, which should help.)
5. Is it easy to control? (I don't have the experience necessary here, but get the impression stepper motors are more complex over DC motors to control, for example)
6. Is it compatible with an Adafruit Motor Shield v2? (This isn't absolutely necessary, but there's quite a bit of documentation and existing examples for using this shield. It would go a LONG way helping me learn to write the code for it if there's great documentation and examples).
7. Can both motors be powered and run off one shield? (I'm looking to control the motors to rotate both module bays at the same time).
I'm currently looking to use a Sparkfun Standard Gearmotor 6RPM (3-12V). It has some excellent torque (Stall Torque: 613 oz-in), is within my price range, and DC motors seem like a decent fit. It seems like it would take approximately 2.5 seconds to rotate the 90 degrees, which I am more than happy with. I'm still lost in a few areas:
1. Is this motor a realistic fit?
2. How can I tell if the Adafruit motor shield can power two of them at once?
3. How do I calculate the type of wall wart to actually power them? (I intend to power them from an outlet nearby, since batteries would require constant monitoring.)
4. If the torque is adequate, can I connect the drive shaft directly to the pivot rod on the module? Is this wise? What is the name of the component I would use exactly?
Any advice would be greatly appreciated.