- Sat Oct 15, 2016 6:38 am
#192032
Hello everyone.I'm new in arduino so I didn't really know how to combine two program into one.
1)Automatic arduino robot (using ultrasonic sensor)
#include <AFMotor.h>
#include <NewPing.h>
#include <Servo.h>
#define TRIG_PIN A4
#define ECHO_PIN A5
#define MAX_DISTANCE 200
#define MAX_SPEED 190 // sets speed of DC motors
#define MAX_SPEED_OFFSET 20
NewPing sonar(TRIG_PIN, ECHO_PIN, MAX_DISTANCE);
AF_DCMotor motor1(1, MOTOR12_1KHZ);
AF_DCMotor motor2(3, MOTOR12_1KHZ);
Servo myservo;
boolean goesForward=false;
int distance = 100;
int speedSet = 0;
void setup() {
myservo.attach(9);
myservo.write(115);
delay(2000);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
}
void loop() {
int distanceR = 0;
int distanceL = 0;
delay(40);
if(distance<=15)
{
moveStop();
delay(100);
moveBackward();
delay(300);
moveStop();
delay(200);
distanceR = lookRight();
delay(200);
distanceL = lookLeft();
delay(200);
if(distanceR>=distanceL)
{
turnRight();
moveStop();
}else
{
turnLeft();
moveStop();
}
}else
{
moveForward();
}
distance = readPing();
}
int lookRight()
{
myservo.write(50);
delay(500);
int distance = readPing();
delay(100);
myservo.write(115);
return distance;
}
int lookLeft()
{
myservo.write(170);
delay(500);
int distance = readPing();
delay(100);
myservo.write(115);
return distance;
delay(100);
}
int readPing() {
delay(70);
int cm = sonar.ping_cm();
if(cm==0)
{
cm = 250;
}
return cm;
}
void moveStop() {
motor1.run(RELEASE);
motor2.run(RELEASE);
}
void moveForward() {
if(!goesForward)
{
goesForward=true;
motor1.run(FORWARD);
motor2.run(FORWARD);
for (speedSet = 0; speedSet < MAX_SPEED; speedSet +=2) // slowly bring the speed up to avoid loading down the batteries too quickly
{
motor1.setSpeed(speedSet);
motor2.setSpeed(speedSet+MAX_SPEED_OFFSET);
delay(5);
}
}
}
void moveBackward() {
goesForward=false;
motor1.run(BACKWARD);
motor2.run(BACKWARD);
for (speedSet = 0; speedSet < MAX_SPEED; speedSet +=2) // slowly bring the speed up to avoid loading down the batteries too quickly
{
motor1.setSpeed(speedSet);
motor2.setSpeed(speedSet+MAX_SPEED_OFFSET);
delay(5);
}
}
void turnRight() {
motor1.run(FORWARD);
motor2.run(BACKWARD);
delay(300);
motor1.run(FORWARD);
motor2.run(FORWARD);
}
void turnLeft() {
motor1.run(BACKWARD);
motor2.run(FORWARD);
delay(300);
motor1.run(FORWARD);
motor2.run(FORWARD);
}
2)Arduino sound sensor(using sound sensor)
//Henry's Bench
//Arduino Sound Detection Sensor Module
int soundDetectedPin = 10; // Use Pin 10 as our Input
int soundDetectedVal = HIGH; // This is where we record our Sound Measurement
boolean bAlarm = false;
unsigned long lastSoundDetectTime; // Record the time that we measured a sound
int soundAlarmTime = 500; // Number of milli seconds to keep the sound alarm high
void setup ()
{
Serial.begin(9600);
pinMode (soundDetectedPin, INPUT) ; // input from the Sound Detection Module
}
void loop ()
{
soundDetectedVal = digitalRead (soundDetectedPin) ; // read the sound alarm time
if (soundDetectedVal == LOW) // If we hear a sound
{
lastSoundDetectTime = millis(); // record the time of the sound alarm
// The following is so you don't scroll on the output screen
if (!bAlarm){
Serial.println("LOUD, LOUD");
bAlarm = true;
}
}
else
{
if( (millis()-lastSoundDetectTime) > soundAlarmTime && bAlarm){
Serial.println("quiet");
bAlarm = false;
}
}
}
Basically what i want to do is to make my robot start to move when it detect any sound using sound sensor.I've been try to combine it many times but still didn't find the right solution.
If anyone can give some time to help me out, i'll be great and thanks very much.
1)Automatic arduino robot (using ultrasonic sensor)
#include <AFMotor.h>
#include <NewPing.h>
#include <Servo.h>
#define TRIG_PIN A4
#define ECHO_PIN A5
#define MAX_DISTANCE 200
#define MAX_SPEED 190 // sets speed of DC motors
#define MAX_SPEED_OFFSET 20
NewPing sonar(TRIG_PIN, ECHO_PIN, MAX_DISTANCE);
AF_DCMotor motor1(1, MOTOR12_1KHZ);
AF_DCMotor motor2(3, MOTOR12_1KHZ);
Servo myservo;
boolean goesForward=false;
int distance = 100;
int speedSet = 0;
void setup() {
myservo.attach(9);
myservo.write(115);
delay(2000);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
distance = readPing();
delay(100);
}
void loop() {
int distanceR = 0;
int distanceL = 0;
delay(40);
if(distance<=15)
{
moveStop();
delay(100);
moveBackward();
delay(300);
moveStop();
delay(200);
distanceR = lookRight();
delay(200);
distanceL = lookLeft();
delay(200);
if(distanceR>=distanceL)
{
turnRight();
moveStop();
}else
{
turnLeft();
moveStop();
}
}else
{
moveForward();
}
distance = readPing();
}
int lookRight()
{
myservo.write(50);
delay(500);
int distance = readPing();
delay(100);
myservo.write(115);
return distance;
}
int lookLeft()
{
myservo.write(170);
delay(500);
int distance = readPing();
delay(100);
myservo.write(115);
return distance;
delay(100);
}
int readPing() {
delay(70);
int cm = sonar.ping_cm();
if(cm==0)
{
cm = 250;
}
return cm;
}
void moveStop() {
motor1.run(RELEASE);
motor2.run(RELEASE);
}
void moveForward() {
if(!goesForward)
{
goesForward=true;
motor1.run(FORWARD);
motor2.run(FORWARD);
for (speedSet = 0; speedSet < MAX_SPEED; speedSet +=2) // slowly bring the speed up to avoid loading down the batteries too quickly
{
motor1.setSpeed(speedSet);
motor2.setSpeed(speedSet+MAX_SPEED_OFFSET);
delay(5);
}
}
}
void moveBackward() {
goesForward=false;
motor1.run(BACKWARD);
motor2.run(BACKWARD);
for (speedSet = 0; speedSet < MAX_SPEED; speedSet +=2) // slowly bring the speed up to avoid loading down the batteries too quickly
{
motor1.setSpeed(speedSet);
motor2.setSpeed(speedSet+MAX_SPEED_OFFSET);
delay(5);
}
}
void turnRight() {
motor1.run(FORWARD);
motor2.run(BACKWARD);
delay(300);
motor1.run(FORWARD);
motor2.run(FORWARD);
}
void turnLeft() {
motor1.run(BACKWARD);
motor2.run(FORWARD);
delay(300);
motor1.run(FORWARD);
motor2.run(FORWARD);
}
2)Arduino sound sensor(using sound sensor)
//Henry's Bench
//Arduino Sound Detection Sensor Module
int soundDetectedPin = 10; // Use Pin 10 as our Input
int soundDetectedVal = HIGH; // This is where we record our Sound Measurement
boolean bAlarm = false;
unsigned long lastSoundDetectTime; // Record the time that we measured a sound
int soundAlarmTime = 500; // Number of milli seconds to keep the sound alarm high
void setup ()
{
Serial.begin(9600);
pinMode (soundDetectedPin, INPUT) ; // input from the Sound Detection Module
}
void loop ()
{
soundDetectedVal = digitalRead (soundDetectedPin) ; // read the sound alarm time
if (soundDetectedVal == LOW) // If we hear a sound
{
lastSoundDetectTime = millis(); // record the time of the sound alarm
// The following is so you don't scroll on the output screen
if (!bAlarm){
Serial.println("LOUD, LOUD");
bAlarm = true;
}
}
else
{
if( (millis()-lastSoundDetectTime) > soundAlarmTime && bAlarm){
Serial.println("quiet");
bAlarm = false;
}
}
}
Basically what i want to do is to make my robot start to move when it detect any sound using sound sensor.I've been try to combine it many times but still didn't find the right solution.
If anyone can give some time to help me out, i'll be great and thanks very much.