- Sun Jun 12, 2016 6:32 am
#190208
Hello,
i have here a Windows 10 OS PC running Processing IDE and an Arduino Pro-mini with a sketch uploaded from the Arduino IDE.
On both the Processing and Arduino i'm running 2 small basic sketches, in purpose to test the BT communication between the Arduino and the PC - the sketches are shown below.
When the Processing code is run (the 'play' button), the Linvor BT dongle red led stops blinking and show it is attached to the PC BT, yet - the motor which is attached to the relay, which is attached to the Arduino, does not start working when pressing the ON button on the Processing sketch window. Motor and relay are working well for sure - i know that, since i put a test function run form setup. i'v tried the same also with HC-06 and HC-05 BT dongles - they all seem to work well and the red led on them stops blinking and shows as if a BT connection is established.
Could the problem be caused by the Windos 10 firewall or anti-virus blocking BT communication? Could it be something else?
Thanks!
Arduino sketch:
#define motorRelay A4
char val; // variable to receive data from the serial port
//int ledpin = 8; // LED connected to pin 48 (on-board LED)
void setup() {
//pinMode(ledpin, OUTPUT); // pin 48 (on-board LED) as OUTPUT
Serial.begin(9600); // start serial communication at 9600bps
pinMode(motorRelay,OUTPUT);
test_motor_before_loop();
}
void test_motor_before_loop(){
digitalWrite(motorRelay,HIGH);
delay(200);
digitalWrite(motorRelay,LOW);
delay(200);
digitalWrite(motorRelay,HIGH);
delay(200);
digitalWrite(motorRelay,LOW);
delay(200);
digitalWrite(motorRelay,HIGH);
delay(200);
}
void loop() {
if( Serial.available() ) // if data is available to read
{
val = Serial.read(); // read it and store it in 'val'
}
if( val == 'H' ) // if 'H' was received
{
digitalWrite(motorRelay, LOW); // turn ON the LED
} else if( val == 'L' ) {
digitalWrite(motorRelay, HIGH); // otherwise turn it OFF
}
delay(100); // wait 100ms for next reading
}
Processing sketch:
// From Arduino Playground tutorial: http://www.arduino.cc/playground/Learning/Tutorial01
//import class to set up serial connection with wiring board
import processing.serial.*;
Serial port;
//button setup
color currentcolor;
RectButton rect1, rect2;
boolean locked = false;
void setup() {
//set up window
size(200, 200);
color baseColor = color(102, 102, 102);
currentcolor = baseColor;
// List all the available serial ports in the output pane.
// You will need to choose the port that the Wiring board is
// connected to from this list. The first port in the list is
// port #0 and the third port in the list is port #2.
println(Serial.list());
// Open the port that the Wiring board is connected to (in this case 1
// which is the second open port in the array)
// Make sure to open the port at the same speed Wiring is at 115200bps (default for BlueSMiRF modem)
port = new Serial(this, Serial.list()[2], 9600); //use the serial device that blueman has setup
// Define and create rectangle button #1
int x = 30;
int y = 100;
int size = 50;
color buttoncolor = color(153, 102, 102);
color highlight = color(102, 51, 51);
rect1 = new RectButton(x, y, size, buttoncolor, highlight);
// Define and create rectangle button #2
x = 90;
y = 100;
size = 50;
buttoncolor = color(153, 153, 153);
highlight = color(102, 102, 102);
rect2 = new RectButton(x, y, size, buttoncolor, highlight);
}
void draw() {
background(currentcolor);
stroke(255);
update(mouseX, mouseY);
rect1.display();
rect2.display();
}
void update(int x, int y) {
if(locked == false) {
rect1.update();
rect2.update();
}
else {
locked = false;
}
//Turn LED on and off if buttons pressed where
//H = on (high) and L = off (low)
if(mousePressed) {
if(rect1.pressed()) { //ON button
currentcolor = rect1.basecolor;
port.write('H');
}
else if(rect2.pressed()) { //OFF button
currentcolor = rect2.basecolor;
port.write('L');
}
}
}
class Button {
int x, y;
int size;
color basecolor, highlightcolor;
color currentcolor;
boolean over = false;
boolean pressed = false;
void update()
{
if(over()) {
currentcolor = highlightcolor;
}
else {
currentcolor = basecolor;
}
}
boolean pressed()
{
if(over) {
locked = true;
return true;
}
else {
locked = false;
return false;
}
}
boolean over()
{
return true;
}
void display()
{
}
}
class RectButton extends Button {
RectButton(int ix, int iy, int isize, color icolor, color ihighlight)
{
x = ix;
y = iy;
size = isize;
basecolor = icolor;
highlightcolor = ihighlight;
currentcolor = basecolor;
}
boolean over()
{
if( overRect(x, y, size, size) ) {
over = true;
return true;
}
else {
over = false;
return false;
}
}
void display()
{
stroke(255);
fill(currentcolor);
rect(x, y, size, size);
}
}
boolean overRect(int x, int y, int width, int height) {
if (mouseX >= x && mouseX <= x+width &&
mouseY >= y && mouseY <= y+height) {
return true;
}
else {
return false;
}
}
i have here a Windows 10 OS PC running Processing IDE and an Arduino Pro-mini with a sketch uploaded from the Arduino IDE.
On both the Processing and Arduino i'm running 2 small basic sketches, in purpose to test the BT communication between the Arduino and the PC - the sketches are shown below.
When the Processing code is run (the 'play' button), the Linvor BT dongle red led stops blinking and show it is attached to the PC BT, yet - the motor which is attached to the relay, which is attached to the Arduino, does not start working when pressing the ON button on the Processing sketch window. Motor and relay are working well for sure - i know that, since i put a test function run form setup. i'v tried the same also with HC-06 and HC-05 BT dongles - they all seem to work well and the red led on them stops blinking and shows as if a BT connection is established.
Could the problem be caused by the Windos 10 firewall or anti-virus blocking BT communication? Could it be something else?
Thanks!
Arduino sketch:
#define motorRelay A4
char val; // variable to receive data from the serial port
//int ledpin = 8; // LED connected to pin 48 (on-board LED)
void setup() {
//pinMode(ledpin, OUTPUT); // pin 48 (on-board LED) as OUTPUT
Serial.begin(9600); // start serial communication at 9600bps
pinMode(motorRelay,OUTPUT);
test_motor_before_loop();
}
void test_motor_before_loop(){
digitalWrite(motorRelay,HIGH);
delay(200);
digitalWrite(motorRelay,LOW);
delay(200);
digitalWrite(motorRelay,HIGH);
delay(200);
digitalWrite(motorRelay,LOW);
delay(200);
digitalWrite(motorRelay,HIGH);
delay(200);
}
void loop() {
if( Serial.available() ) // if data is available to read
{
val = Serial.read(); // read it and store it in 'val'
}
if( val == 'H' ) // if 'H' was received
{
digitalWrite(motorRelay, LOW); // turn ON the LED
} else if( val == 'L' ) {
digitalWrite(motorRelay, HIGH); // otherwise turn it OFF
}
delay(100); // wait 100ms for next reading
}
Processing sketch:
// From Arduino Playground tutorial: http://www.arduino.cc/playground/Learning/Tutorial01
//import class to set up serial connection with wiring board
import processing.serial.*;
Serial port;
//button setup
color currentcolor;
RectButton rect1, rect2;
boolean locked = false;
void setup() {
//set up window
size(200, 200);
color baseColor = color(102, 102, 102);
currentcolor = baseColor;
// List all the available serial ports in the output pane.
// You will need to choose the port that the Wiring board is
// connected to from this list. The first port in the list is
// port #0 and the third port in the list is port #2.
println(Serial.list());
// Open the port that the Wiring board is connected to (in this case 1
// which is the second open port in the array)
// Make sure to open the port at the same speed Wiring is at 115200bps (default for BlueSMiRF modem)
port = new Serial(this, Serial.list()[2], 9600); //use the serial device that blueman has setup
// Define and create rectangle button #1
int x = 30;
int y = 100;
int size = 50;
color buttoncolor = color(153, 102, 102);
color highlight = color(102, 51, 51);
rect1 = new RectButton(x, y, size, buttoncolor, highlight);
// Define and create rectangle button #2
x = 90;
y = 100;
size = 50;
buttoncolor = color(153, 153, 153);
highlight = color(102, 102, 102);
rect2 = new RectButton(x, y, size, buttoncolor, highlight);
}
void draw() {
background(currentcolor);
stroke(255);
update(mouseX, mouseY);
rect1.display();
rect2.display();
}
void update(int x, int y) {
if(locked == false) {
rect1.update();
rect2.update();
}
else {
locked = false;
}
//Turn LED on and off if buttons pressed where
//H = on (high) and L = off (low)
if(mousePressed) {
if(rect1.pressed()) { //ON button
currentcolor = rect1.basecolor;
port.write('H');
}
else if(rect2.pressed()) { //OFF button
currentcolor = rect2.basecolor;
port.write('L');
}
}
}
class Button {
int x, y;
int size;
color basecolor, highlightcolor;
color currentcolor;
boolean over = false;
boolean pressed = false;
void update()
{
if(over()) {
currentcolor = highlightcolor;
}
else {
currentcolor = basecolor;
}
}
boolean pressed()
{
if(over) {
locked = true;
return true;
}
else {
locked = false;
return false;
}
}
boolean over()
{
return true;
}
void display()
{
}
}
class RectButton extends Button {
RectButton(int ix, int iy, int isize, color icolor, color ihighlight)
{
x = ix;
y = iy;
size = isize;
basecolor = icolor;
highlightcolor = ihighlight;
currentcolor = basecolor;
}
boolean over()
{
if( overRect(x, y, size, size) ) {
over = true;
return true;
}
else {
over = false;
return false;
}
}
void display()
{
stroke(255);
fill(currentcolor);
rect(x, y, size, size);
}
}
boolean overRect(int x, int y, int width, int height) {
if (mouseX >= x && mouseX <= x+width &&
mouseY >= y && mouseY <= y+height) {
return true;
}
else {
return false;
}
}