- Sun Mar 13, 2016 10:20 am
#188659
Hey,
For my project I am using 18x a 8mm flat micro DC motor. I have arranged the motors so that they are divided into 6 sections (6 sections of 3 motors). Each motor in the section works together. Using the same positive and negative leads. Each motor draws current of 70mA (total of 210mA for each section). Each section is connected to a PWM pin, so that I can code to increase the vibration speed. Although, the Arduino only outputs a total of 40mA for each pin.
I have tried using the FQP30N06 transistor for each section. Following the setup by connecting the gate to the i/o pin, on the Arduino; the source to the common ground, and then drain to an external 9v battery. I was able to set-up the first 2-4 transistors for their sections, but once I came to setup the transistors fro the 4-6 the motors would run automatically. I tried setting it up by not putting the source into the common ground for a couple of them. That did the trick, but then I couldn't control those sections. So I went to put them back in the common ground and all the motors would run, almost like they where putting power back into the Arduino, turning it on and triggering them to all turn on.
What is a viable solution to run 18 vibration motors?
Can I fix the problem with using a transistor for each section?
Could I use a ULN2803A transitor to control all of the sections?
Thanks a lot!!
For my project I am using 18x a 8mm flat micro DC motor. I have arranged the motors so that they are divided into 6 sections (6 sections of 3 motors). Each motor in the section works together. Using the same positive and negative leads. Each motor draws current of 70mA (total of 210mA for each section). Each section is connected to a PWM pin, so that I can code to increase the vibration speed. Although, the Arduino only outputs a total of 40mA for each pin.
I have tried using the FQP30N06 transistor for each section. Following the setup by connecting the gate to the i/o pin, on the Arduino; the source to the common ground, and then drain to an external 9v battery. I was able to set-up the first 2-4 transistors for their sections, but once I came to setup the transistors fro the 4-6 the motors would run automatically. I tried setting it up by not putting the source into the common ground for a couple of them. That did the trick, but then I couldn't control those sections. So I went to put them back in the common ground and all the motors would run, almost like they where putting power back into the Arduino, turning it on and triggering them to all turn on.
What is a viable solution to run 18 vibration motors?
Can I fix the problem with using a transistor for each section?
Could I use a ULN2803A transitor to control all of the sections?
Thanks a lot!!