- Mon Jul 06, 2015 9:21 am
#183190
Hi all,
I am interfacing an RN-XV to an older PC at 2400 baud. It works perfectly, no data is dropped when connected directly. Not using flow control.
However, I'd like to introduce an Arduino Uno (actually, a MicroView) into the middle of the setup to eventually do some real-time data translation. This mostly works, but when there is a large burst of incoming data, a few characters get dropped and the data gets a slightly garbled, but it does recover.
Helpful diagram:
Code:
Any suggestions?
I am interfacing an RN-XV to an older PC at 2400 baud. It works perfectly, no data is dropped when connected directly. Not using flow control.
However, I'd like to introduce an Arduino Uno (actually, a MicroView) into the middle of the setup to eventually do some real-time data translation. This mostly works, but when there is a large burst of incoming data, a few characters get dropped and the data gets a slightly garbled, but it does recover.
Helpful diagram:
Code:
Code: Select all
Nothing to it, right? I'm having a hard time believing that the Uno can't keep up, especially at such a low baud rate, but I'm sure there are background issues with interrupts and so on introduced by SoftwareSerial. Initial guess is that a buffer is filling up somewhere, but I'm not an expert on the innards.#include <SoftwareSerial.h>
SoftwareSerial mySerial(8, 9); // RX, TX
void setup()
{
Serial.begin(2400);
mySerial.begin(2400);
}
void loop() // run over and over
{
if (mySerial.available())
Serial.write(mySerial.read());
if (Serial.available())
mySerial.write(Serial.read());
}
Any suggestions?