- Fri Sep 05, 2014 5:18 am
#174564
I managed to run a bipolar motor using an H-Bridge driver module, however the motor operates slowly.
When I connect the batteries directly to the motor, it operates well.
What might be the problem ?
Details:
When I connect the batteries directly to the motor, it operates well.
What might be the problem ?
Details:
- The driver module:
http://www.ebay.com/itm/Duel-H-Bridge-L ... 1167572579 - Arduino UNO
- Voltage Input to the driver module:
Six 1.5V AA normal batteries (a few brands).
The batteries are not full, so I get approx 8V input - Voltage input to the Arduino:
standard GP 9V batery.