- Sat Jun 22, 2013 5:29 pm
#160825
Hello,
I made one project with my arduino, one lcd16x2, 4 led segments... and i want use the 12v from the car lighter to power the Arduino\circuit.. what is the better way to do this?
Its better if i buy something like this:
DC-DC Converter Board Voltage Regulator Stepdown Module [LM2596S]
Specifications:
Input Voltage: 3-30VDC
Output voltage: 1.21-18VDC
Max output current: 3A (Recommend use following in 2A, leaving a certain margin)
Built in LM2596S-adj
Dimensions: 37mm x 37mm
Step-down: The input voltage must be at least 1.5v higher than the output voltage.
Thank you
I made one project with my arduino, one lcd16x2, 4 led segments... and i want use the 12v from the car lighter to power the Arduino\circuit.. what is the better way to do this?
Its better if i buy something like this:
DC-DC Converter Board Voltage Regulator Stepdown Module [LM2596S]
Specifications:
Input Voltage: 3-30VDC
Output voltage: 1.21-18VDC
Max output current: 3A (Recommend use following in 2A, leaving a certain margin)
Built in LM2596S-adj
Dimensions: 37mm x 37mm
Step-down: The input voltage must be at least 1.5v higher than the output voltage.
Thank you