I also tried using void, but it was of no use. policelights() was in the same program.
Code: Select all
#include <SoftwareSerial.h>
#include <TinyGPS.h>
#define NUM_OFF 2
#define DELAY 50
#define TEST_BUTTON 9
#define DEFAULT_SPEED_LIMIT 5
#define NSPEEDZONES 6
boolean debugMode = true;
boolean speeding = false;
int blue;
class Vertex {
public:
Vertex(float llat, float llng) {
lat = llat;
lng = llng;
}
float lat;
float lng;
};
class SpeedZone {
public:
SpeedZone(int s) {
speedLimit = s;
}
void setVertices(int n, Vertex *v) {
nVertices = n;
vertices = v;
}
int nVertices;
Vertex *vertices;
int speedLimit;
};
SpeedZone *speedZones[NSPEEDZONES];
TinyGPS gps;
SoftwareSerial nss(3, 4);
boolean buttonPressed = false;
SoftwareSerial cell(7,8); // We need to create a serial port on D2/D3 to talk to the GSM module
char mobilenumber[] = "XXXXXXXXXXX";
void setup() {
Serial.begin(9600);
setupSpeedZones();
blue = 12;
pinMode(blue, OUTPUT);
pinMode(TEST_BUTTON, INPUT);
digitalWrite(TEST_BUTTON, HIGH);
cell.begin(4800);
delay(3500); // give the GSM module time to initialise, locate network etc.
delay(3000);
nss.begin(9600);
}
void setupSpeedZones() {
// 2nd main road
speedZones[0] = &SpeedZone(25);
speedZones[0]->setVertices(12, (Vertex[12]){
Vertex(12.943427649396137, 77.53860712051392),
Vertex(12.942570236686135, 77.53871440887451),
Vertex(12.94140958795451,77.53876805305481),
Vertex(12.940980878498074, 77.53875732421875),
Vertex(12.940353497477103, 77.5388753414154),
Vertex(12.939046448613755,77.5390899181366 ),
Vertex(12.938021717514202,77.53932595252991 ),
Vertex(12.937760305845364,77.53974437713623 ),
Vertex(12.93687150412194,77.53973364830017 ),
Vertex(12.935982699231385,77.53956198692322 ),
Vertex(12.934142340214253,77.53906846046448),
Vertex(12.933943664281175,77.538982629776 )});
// 80 feet Double Road
speedZones[1] = &SpeedZone(15);
speedZones[1]->setVertices(9, (Vertex[9]){
Vertex(12.941044923555157, 77.53885790705681),
Vertex(12.941039695387857, 77.53906175494194),
Vertex(12.941035774262303, 77.5392173230648),
Vertex(12.941027932011004, 77.53935679793358),
Vertex(12.940876315104193, 77.54202961921692),
Vertex(12.94081357704682, 77.54283428192139),
Vertex(12.940698557233977, 77.54501223564148),
Vertex(12.94058353736807,77.54695415496826 ),
Vertex(12.940520799237047, 77.54763007164001)});
// Block road
speedZones[2] = &SpeedZone(10);
speedZones[2]->setVertices(16, (Vertex[16]){
Vertex(12.933547619021462,77.53549307584763),
Vertex(12.93361689431027,77.53550313413143 ),
Vertex(12.933661988591705,77.5354977697134),
Vertex(12.933694012061984,77.53548838198185),
Vertex(12.933777665189446,77.53545552492142),
Vertex(12.933820798822312,77.5354354083538),
Vertex(12.933860664749114,77.53541797399521),
Vertex(12.934049537659947,77.53533147275448),
Vertex(12.93419985163906,77.53525167703629),
Vertex(12.934398527368137,77.53516852855682),
Vertex(12.934513550086338,77.53511488437653),
Vertex(12.934594588787776,77.53507733345032),
Vertex(12.93473575291451,77.53501027822495),
Vertex(12.934853389625761,77.53495931625366),
Vertex(12.934952727249843,77.5349110364914),
Vertex(12.934984097017653,77.53490567207336)});
// towards post office
speedZones[3] = &SpeedZone(35);
speedZones[3]->setVertices(20, (Vertex[20]){
Vertex(12.93382341298164, 77.53911674022675),
Vertex(12.933729303228546, 77.53927633166313),
Vertex(12.933663949212452, 77.53939434885979),
Vertex(12.933615587229529, 77.5394868850708),
Vertex(12.933513634910476,77.53962635993958 ),
Vertex(12.9334495879195, 77.5397376716137),
Vertex(12.933313651394398, 77.53990530967712),
Vertex(12.933197321040067, 77.54006892442703),
Vertex(12.933090140216153, 77.54023790359497),
Vertex(12.933005179774247, 77.54036530852318),
Vertex(12.932905841374719, 77.54049941897392),
Vertex(12.932785589574985, 77.54066303372383),
Vertex(12.932637888915574, 77.54087224602699),
Vertex(12.932517636986722, 77.54102379083633),
Vertex(12.932401306261246, 77.54119008779526),
Vertex(12.932307195971756, 77.54131078720093),
Vertex(12.932219621087134, 77.54143953323364),
Vertex(12.932149038321938, 77.54154548048973),
Vertex(12.93218171553054, 77.54162460565567),
Vertex(12.932209164382444, 77.54164338111877)});
// ring road
speedZones[4] = &SpeedZone(40);
speedZones[4]->setVertices(11, (Vertex[11]){
Vertex(12.933744988189858, 77.53884315490723),
Vertex(12.93417371008398, 77.53815650939941),
Vertex(12.934696540665088, 77.53731966018677),
Vertex(12.935062521419919, 77.53671884536743),
Vertex(12.935313479341485, 77.53631114959717),
Vertex(12.935648089510861, 77.53558158874512),
Vertex(12.936087264677003, 77.53476619720459),
Vertex(12.936599634726921, 77.53420829772949),
Vertex(12.937321133624925, 77.53389716148376),
Vertex(12.937948522274533, 77.53362894058228),
Vertex(12.938230846651972, 77.53344655036926)});
// new road
speedZones[5] = &SpeedZone(30);
speedZones[5]->setVertices(11, (Vertex[11]){
Vertex(12.943443333747508, 77.5386044383049),
Vertex(12.943435491571943, 77.53841936588287),
Vertex(12.943432877513375, 77.53809481859207),
Vertex(12.943432877513375, 77.53791779279709),
Vertex(12.943425035337478, 77.53762006759644),
Vertex(12.943417193161341, 77.53743767738342),
Vertex(12.943409350984949, 77.53721237182617),
Vertex(12.943411965043772, 77.53708630800247),
Vertex(12.943406736926102, 77.53692269325256),
Vertex(12.94338582445431, 77.53680735826492),
Vertex(12.943357069802731, 77.53675907850266)});
if (debugMode) {
printSpeedZones();
}
}
boolean inSpeedZone(int speedZone, float lat, float lng) {
SpeedZone *s = speedZones[speedZone];
int i, j;
boolean inside = false;
for (i = 0, j = s->nVertices-1; i < s->nVertices; j = i++) {
if ( ((s->vertices[i].lat > lat) != (s->vertices[j].lat > lat)) &&
(lng < (s->vertices[j].lng - s->vertices[i].lng) * (lat - s->vertices[i].lat) / (s->vertices[j].lat - s->vertices[i].lat) + s->vertices[i].lng) )
inside = !inside;
}
return inside;
}
boolean inSpeedZone(int speedZone) {
float lat, lng;
unsigned long fix_age;
// retrieves +/- lat/long in 100,000ths of a degree
gps.f_get_position(&lat, &lng, &fix_age);
return inSpeedZone(speedZone, lat, lng);
}
void loop() {
if (readGPS()) {
if (debugMode) {
debug();
}
speeding = isSpeeding();
}
if (digitalRead(TEST_BUTTON) == LOW) {
buttonPressed = true;
} else {
buttonPressed = false;
}
if ((speeding || buttonPressed) && (!(speeding && buttonPressed))) {
policeLights();
} else {
allOff();
}
}
bool readGPS() {
while (nss.available()) {
if (gps.encode(nss.read())) {
return true;
}
}
return false;
}
int getSpeedLimit() {
boolean isInSpeedZone;
for(int i=0;i<NSPEEDZONES;i++) {
isInSpeedZone = inSpeedZone(i);
if (isInSpeedZone) {
return speedZones[i]->speedLimit;
}
}
return DEFAULT_SPEED_LIMIT;
}
boolean isSpeeding() {
int speed = (int)(gps.f_speed_kmph() + 0.5);
int speedLimit = getSpeedLimit();
if (speed > speedLimit) {
delay (5000);
if (speed > speedLimit)
return true;
}
return false;
}
void policeLights() {
digitalWrite(blue, HIGH);
cell.println("AT+CMGF=1"); // set SMS mode to text
cell.print("AT+CMGS="); // now send message...
cell.write((byte)34); // ASCII equivalent of "
cell.print(mobilenumber);
cell.write((byte)34); // ASCII equivalent of "
cell.println();
delay(500); // give the module some thinking time
cell.print("hi bobby, the king of kings... :-)"); // our message to send
cell.write((byte)26); // ASCII equivalent of Ctrl-Z
cell.println();
delay(15000); // the SMS module needs time to return to OK status
return;
}
void allOff() {
digitalWrite(blue,LOW);
}
void printSpeedZones() {
for(int i=0;i<NSPEEDZONES;i++) {
SpeedZone *s = speedZones[i];
Serial.println(s->speedLimit);
for(int v=0;v<s->nVertices;v++) {
Serial.print("(");
Serial.print(s->vertices[v].lat,15);
Serial.print(", ");
Serial.print(s->vertices[v].lng,15);
Serial.println(")");
}
}
}
void debug() {
float lat, lng;
unsigned long fix_age, time, date, speed, course;
// retrieves +/- lat/long in 100000ths of a degree
gps.f.get_position(&lat, &lng, &fix_age);
Serial.println(getSpeedLimit());
Serial.print("lat: ");
Serial.print(lat,15);
Serial.print(" lng: ");
Serial.print(lng,15);
Serial.print(" speed: ");
Serial.println(gps.f_speed_kmph());
}
i have removed do while...still problem persists.
This code checks for the current location (using gps module) and accesses the speed limit set in the speedzone defined in the program, and sends a message to the police if speedlimit of a road is exceeded.
I have used 15 digits after the decimal point in lat and long values defined in the program. Will arduino process so many digits??
I am using arduino uno.