Arduino Control of Electronic Speed Control (ESC)
Posted: Mon Apr 02, 2012 11:23 am
Hi -
I am spending some time looking at how an Arduino can be used to control a brushless motor. I am using an Arduino Duemilanove, a Hacker x-5 Pro ESC, and a Hacker A-10 brushless motor.
I am able to both arm the ESC and use it to operate the motor, but I am running into a few items that I don't quite understand that are mostly related to using the Servo library.
I have read through a previous discussion and have most items figured out, but I wanted to post my sketches and get some feedback.
This first sketch is used to arm the ESC and works as expected:
I then wrote the following sketch to use the servo function to arm the ESC. This code works, but does not behave as the arm sketch above. This sketch arms the ESC, but if I then turn the power to the ESC off and then on, the ESC rearms without the sketch being run again. So something going on with the myservo.write that I am not getting...
I am spending some time looking at how an Arduino can be used to control a brushless motor. I am using an Arduino Duemilanove, a Hacker x-5 Pro ESC, and a Hacker A-10 brushless motor.
I am able to both arm the ESC and use it to operate the motor, but I am running into a few items that I don't quite understand that are mostly related to using the Servo library.
I have read through a previous discussion and have most items figured out, but I wanted to post my sketches and get some feedback.
This first sketch is used to arm the ESC and works as expected:
Code: Select all
This second sketch adds to the first one and both arms the ESC and then provides a pulse train to operate the motor at a constant speed. This also works as expected.// This sketch arms the Hacker X-5 Pro ESC
int escPin = 9;
int arm = 1000; // pulse width in microseconds (Start Signal)
void setup()
{
// It appears that the ESC will accept a range of values for the arming
// sequence. This provides 10 pulses with a pulse width of 1000 us with
// with a 20 ms delay between pulses.
pinMode(escPin, OUTPUT);
for (int count = 0; count < 10; count++){
digitalWrite(escPin, HIGH);
delayMicroseconds(arm);
digitalWrite(escPin, LOW);
delay(20);
}
}
void loop()
{
}
Code: Select all
I would be happy with this, but I have looked over some forums and find many mentions of using the Servo library to control the ESC/motor combination. The only problem is that the only sketches that I can find refer to the Servo Sweep sketch that runs the motor speed up and down. If I arm the ESC using the above sketch and then upload the Sweep sketch to the Arduino, the motor runs as expected with the speed oscillating up and down.// This sketch arms the Hacker X-5 Pro ESC and
// then runs the attached A-10 Hacker brushless motor
// at a constant speed.
int escPin = 9;
int arm = 1000; // pulse width in microseconds for arming
int speedvalue = 1350; // pulse width in microseconds for operation
void setup()
{
// It appears that the ESC will accept a range of values for the arming
// sequence. This provides 10 pulses with a pulse width of 1000 us with
// with a 20 ms delay between pulses.
pinMode(escPin, OUTPUT);
for (int count = 0; count < 10; count++){
digitalWrite(escPin, HIGH);
delayMicroseconds(arm);
digitalWrite(escPin, LOW);
delay(20);
}
}
void loop()
{
// Once armed the ESC needs to receive a pulse train to operate the
// the motor. The motor speed is controlled by the duration of the
// pulse width.
// This simple loop provides a pulses width a width of 1350 us and a
// separation of 20 ms.
digitalWrite(escPin, HIGH);
delayMicroseconds(speedvalue);
digitalWrite(escPin, LOW);
delay(20);
}
I then wrote the following sketch to use the servo function to arm the ESC. This code works, but does not behave as the arm sketch above. This sketch arms the ESC, but if I then turn the power to the ESC off and then on, the ESC rearms without the sketch being run again. So something going on with the myservo.write that I am not getting...
Code: Select all
This last sketch arms the ESC using the servo functions but does not result in operation of the motor. I would be okay with this except that when I look at the pulse train on a scope, they look virtually identical. I have just read that the ESC may need to run from zero up to the desired speed which mimics the action of an RC controller - this makes sense and I will try it later today. // This sketch uses the servo library to arm the Hacker X-5 Pro ESC.
// Once loaded this code will rearm the ESC after its power has been
// turned off and on without being re-run.
// What is going on????
#include <Servo.h>
Servo myservo;
int arm = 46; // supplies a pulse width of approximately 1000 us
void setup()
{
myservo.attach(9);
for (int count = 0; count < 10; count++){
myservo.write(arm);
}
}
void loop()
{
}
Code: Select all
If any one has any insight to what is going one within the code, I would appreciate your feedback. I would also be interested in seeing a sketch that uses the servo library to operate the ESC/motor at a constant speed.// This sketch uses the servo library to arm the Hacker X-5 Pro ESC.
// Once loaded this code will rearm the ESC after its power has been
// turned off and on without being re-run.
// What is going on????
#include <Servo.h>
Servo myservo;
int arm = 46; // supplies a pulse width of approximately 1000 us
int speedvalue = 100; // supplies a pulse width of approximatley 1350 us
void setup()
{
myservo.attach(9);
for (int count = 0; count < 10; count++){
myservo.write(arm);
}
}
void loop()
// This loop produces a pulse train but it does not result in
// the ESC operating the brusless motor.
{
myservo.write(speedvalue);
}