- Wed Feb 23, 2011 10:49 am
#121051
It's actually a 60VDC servo motor. The servo drive accepts 5V step and direction inputs. Power supply to the motor goes through the drive. We build systems with both servos and steppers. Both the servo and stepper drives that we use accept step/direction. In order to get acceptable performance, I need a 25Khz pulse rate. We drive these right now using a PC parallel port. The Arduino will just replace the PC in this simple application (push a button and move to a limit switch, wait a set time, then move back to the home position).
I'm basically using the Arduino as a programmable pulse generator...As long as it can pulse fast enough. We would typically use a PLC for this which can pulse at 10Khz (25Khz with an expensive high speed IO module). I'm experimenting with the Arduino as a low cost alternative for cost sensitive applications.