- Thu Jun 21, 2018 10:06 pm
#199520
Hello everyone,
I'm having a lot of difficulty getting the Tiny AVR Programmer, aka (PMG-11801) to work on my Ubuntu 18.04 laptop. I have read several forum posts from various places and tried a solution that looks like it out to work but it has not. Here's what I've done.
From various web pages it seems like I need an entry in /etc/udev/rules.d to allow permission to use this device. I added it and it looks like this
Thank you.
-mike
I'm having a lot of difficulty getting the Tiny AVR Programmer, aka (PMG-11801) to work on my Ubuntu 18.04 laptop. I have read several forum posts from various places and tried a solution that looks like it out to work but it has not. Here's what I've done.
Code: Select all
I note the 1781:0c9fmmachenry$ lsusb
...
Bus 001 Device 013: ID 1781:0c9f Multiple Vendors USBtiny
...
From various web pages it seems like I need an entry in /etc/udev/rules.d to allow permission to use this device. I added it and it looks like this
mmachenry$ cat /etc/udev/rules.d/99-USBtiny.rulesAlso note that I'm in the proper group.
SUBSYSTEM=="usb", ATTR{idVendor}=="1781", ATTR{idProduct}=="0c9f", GROUP="adm", MODE="0666"
Code: Select all
I also ran these immediately after creating that rules file.mmachenry$ groups
mmachenry adm dialout cdrom sudo dip plugdev docker lpadmin sambashare
Code: Select all
But when I run avrdude, I get permission denied.sudo service udev restart
sudo udevadm control --reload-rules
Code: Select all
However, I get much different, positive output when running the command with sudo.mmachenry$ hardware/tools/avr/bin/avrdude -C/home/mmachenry/Downloads/arduino-1.8.5-linux64/arduino-1.8.5/hardware/tools/avr/etc/avrdude.conf -vv -pattiny85 -cusbtiny
avrdude: Version 6.3, compiled on Jan 17 2017 at 11:00:16
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "/home/mmachenry/Downloads/arduino-1.8.5-linux64/arduino-1.8.5/hardware/tools/avr/etc/avrdude.conf"
User configuration file is "/home/mmachenry/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : usb
Using Programmer : usbtiny
avrdude: usbdev_open(): Found USBtinyISP, bus:device: 001:013
avrdude: Warning: cannot open USB device: Permission denied
avrdude: Error: Could not find USBtiny device (0x1781/0xc9f)
avrdude done. Thank you.
Code: Select all
Why is the permission for a regular user to access this device still denied? By the way this works on my friend's Mac and another friend's Windows machine so I know that the programmer and the ATTiny85 in it are function just fine and not damaged.sudo hardware/tools/avr/bin/avrdude -C/home/mmachenry/Downloads/arduino-1.8.5-linux64/arduino-1.8.5/hardware/tools/avr/etc/avrdude.conf -vv -pattiny85 -cusbtiny
avrdude: Version 6.3, compiled on Jan 17 2017 at 11:00:16
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "/home/mmachenry/Downloads/arduino-1.8.5-linux64/arduino-1.8.5/hardware/tools/avr/etc/avrdude.conf"
User configuration file is "/home/mmachenry/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : usb
Using Programmer : usbtiny
avrdude: usbdev_open(): Found USBtinyISP, bus:device: 001:013
AVR Part : ATtiny85
Chip Erase delay : 400000 us
PAGEL : P00
BS2 : P00
RESET disposition : possible i/o
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 12 4 0 no 512 4 0 4000 4500 0xff 0xff
flash 65 6 32 0 yes 8192 64 128 30000 30000 0xff 0xff
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
lock 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
lfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
efuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
Programmer Type : USBtiny
Description : USBtiny simple USB programmer, http://www.ladyada.net/make/usbtinyisp/
avrdude: programmer operation not supported
avrdude: Using SCK period of 10 usec
CMD: [ac 53 00 00] [ac 52 53 00]
avrdude: AVR device initialized and ready to accept instructions
Reading | | 0% 0.00sCMD: [30 00 00 00] [00 30 00 1e]
CMD: [30 00 01 00] [00 30 00 93]
Reading | ################# | 33% 0.00sCMD: [30 00 02 00] [00 30 00 0b]
Reading | ################################################## | 100% 0.00s
avrdude: Device signature = 0x1e930b (probably t85)
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [58 08 00 00] [00 58 08 df]
CMD: [58 08 00 00] [00 58 08 df]
CMD: [58 08 00 00] [00 58 08 df]
avrdude: safemode: hfuse reads as DF
CMD: [50 08 00 00] [00 50 08 ff]
CMD: [50 08 00 00] [00 50 08 ff]
CMD: [50 08 00 00] [00 50 08 ff]
avrdude: safemode: efuse reads as FF
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [50 00 00 00] [00 50 00 e2]
CMD: [58 08 00 00] [00 58 08 df]
CMD: [58 08 00 00] [00 58 08 df]
CMD: [58 08 00 00] [00 58 08 df]
avrdude: safemode: hfuse reads as DF
CMD: [50 08 00 00] [00 50 08 ff]
CMD: [50 08 00 00] [00 50 08 ff]
CMD: [50 08 00 00] [00 50 08 ff]
avrdude: safemode: efuse reads as FF
avrdude: safemode: Fuses OK (E:FF, H:DF, L:E2)
avrdude done. Thank you.
Thank you.
-mike