SparkFun Forums 

Where electronics enthusiasts find answers.

Questions relating to designing PCBs
By solex
#38036
Hello all,

I have finished my board, used the files in the eagle tutorials and generated the gerbers. But when I look in the folder they are supposed to be in according to the headder of eagle cad there not there!

All I find is eagle.epf :s

Any help would be great!

Charles
User avatar
By bigglez
#38047
solex wrote:I have finished my board, used the files in the eagle tutorials and generated the gerbers. But when I look in the folder they are supposed to be in according to the headder of eagle cad there not there! All I find is eagle.epf
Greetings Charles,

Are you on a Windows platform? Output files are stored in the
sub-dir where you started the project. An eagle.epf file only
contains the project specific settings.

Go back to the schematic editor and do a "Save as", this will
point to the directory where your outputs goes. Or, do a search
for one of the expected files (*.cmp for example).

A correctly executed project from EAGLE will contain:

*.cmp
*.drd
*.dri
*.drl
*.erc
*.gpi
*.plc
*.pls
*.sch
*.silk
*.sol
*.stc
*.sts

Comments Welcome!
By solex
#38048
Yes I am using windows. I am looking in the sub directory where I have save as 'd the files, but yet its notcoming up...
User avatar
By bigglez
#38049
solex wrote:Yes I am using windows. I am looking in the sub directory where I have save as 'd the files, but yet its notcoming up...
Greetings Charles,

You should see at least the *.sch, and if you've attempted
a board design the *.brd.

Can you do a windows search for the *.sch and *.brd?

What other files are in the sub dir where EAGLE is pointing?

Comments Welcome!
By solex
#38052
Ive found the files, but they seem to be in

C:\Users\*****\AppData\Local\VirtualStore\Program Files\EAGLE-4.16r2\Projects


Not sure what to touch so I dont loose any thing, any suggestions?

Charles
User avatar
By bigglez
#38056
solex wrote:Ive found the files, but they seem to be in

C:\Users\*****\AppData\Local\VirtualStore\Program Files\EAGLE-4.16r2\Projects

Not sure what to touch so I dont loose any thing, any suggestions?
Greetings Charles,

Good to hear that you have not lost any work. The place where
EAGLE stores files can be changed to suit your needs.

As you can see, EAGLE spawns many files as the work
progresses, so it's wise to organize your work.

EAGLE provides a folder (sub-dir) structure called Projects.

You should also have a pdf tutorial that will help you
understand how EAGLE works (most of us found it to be
far from intuitive!).

Get a copy of the tutorialhere.

Comments Welcome!
By solex
#38057
Thats the thing, They are "saved" in the normal location, and if I save as in the location there supposed to be in *the place you just refranced* and if i click open it shows me the folder where they are supposed to be but its far from empty if I use windows exporor to look in it, *oer dos for that measure, thought I should check old school ;)*

It seemd like eagle is thinking it is saving and loading from the correct location but is saving and opening from the one I gave you... Will grab my files and reinstall eagle, hope that sorts it out :)

Thank you for your help

Charles
By Azoore
#38061
It sounds like you're using Vista. Vista prevents programs from writing to protected system folders, such as Program Files. Eagle is one program that does this by default (tisk tisk cadsoft). Instead, Vista will place those saved files in the VirtualStore folder.
By solex
#38104
Yes I am. I stumbled across the default folders settings, so if I reinstall and set these to some where other than Program Files it should be fine?

Thank you both

Charles
By Azoore
#38126
Yep.
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]