- Fri Nov 09, 2007 12:25 pm
#37802
Hi, I'm working on a small board design using the GR-10 GPS receiver and the GPS chipscale antenna. In the datasheet for the antenna it mentions a 50ohm microstrip, I'm only vaguely familiar with microstrip traces - I understand the idea is to have a controlled-impedance trace, and I used a free online calculator to get the proper trace width, but I have some questions.
First, does the trace length matter? In the datasheet they give a specific length for the trace and I'm wondering if I need to match that, or if it can be any length?
Also, am I correct in assuming that microstrip should connect to the ANT pin on the GR-10, and if so, is it reasonable to assume that if I need to make a 90degree turn in the trace, I should do two 45-degree turns instead, to reduce impedance changes?
Lastly, should I have a stop layer over the microstrip so there is no solder mask over it, or is soldermask okay?
Thanks very much!
First, does the trace length matter? In the datasheet they give a specific length for the trace and I'm wondering if I need to match that, or if it can be any length?
Also, am I correct in assuming that microstrip should connect to the ANT pin on the GR-10, and if so, is it reasonable to assume that if I need to make a 90degree turn in the trace, I should do two 45-degree turns instead, to reduce impedance changes?
Lastly, should I have a stop layer over the microstrip so there is no solder mask over it, or is soldermask okay?
Thanks very much!