- Fri Nov 02, 2007 9:46 am
#37438
I knew mentor graphic PADs has a toolset to convert files from different vendors, but never see one myself.
Where electronics enthusiasts find answers.
jasonharper wrote:propellanttech wrote:I could use some feedback on what software other people are using to design their boards.I use Osmond PCB, for Macintosh. It produces standard Gerber files, including a solder paste layer (I normally send that off to Pololu to get a laser-cut mylar paste stencil made).
It also produces a file called PIK.TXT, containing pick-and-place data. Here's the first few lines from one:Code: Select all(the file is actually tab-delimited, it's probably not going to look too good here.) It seems like that would be exactly what you needed, except for one thing - many of the footprints in Osmond's libraries are defined with the origin at pin 1 rather than the center of the part, and I think it's the origin being reported here. I suspect I would have to fix that for every footprint I use before the file would be of any use to you.Designator Part Midx Midy Refx Refy Padx Pady TB Rotation U2 SOT23-6 0.963 1.231 0.963 1.231 0.963 1.231 Top 0.0 C1 0805 0.750 0.875 0.750 0.875 0.750 0.875 Top -90.0
OT wrote:I have read this thread with interest, and although I must say have yet to make any devices that have not been hard wired, and surface mount devices is limited to breakout boards, this service together with batch pcb might be the push to needed to learn Eagle and get going. Would 20-28 pin QFNs represent any problem?
What about a design like this (gerber files for nRF24L01 module): http://www.nordicsemi.com/index_popup.c ... 9&prop=550
With no cutting services, what alternatives could be pointed to for small boards like that?
jasonharper wrote:Took a look at your FAQ... your contact info shows an address in the USA, but your site has a .NZ domain, so I have to ask: What country would I be shipping parts to? What currency are your quoted prices in?
Also, what exactly are your requirements for fiducials? I found some info on the subject at http://www.tkb-4u.com/articles/other/fi ... ducial.php, which shows several commonly used shapes - are all of them compatible with your equipment?
busonerd wrote:James,
Just took a look at your site, You mention FPGA's as something you can't visually inspect, do you perhaps mean BGA / FBGA / FTBGA / CSP?
FPGA's are also a type of chip, and they come in PQFP packages too.
Cheers,
--David Carne
b_w_ wrote:James-Brian,
I am very excited by the potential of your service. I have been using BatchPCB for a couple years now but have always stuck to through hole components in my work. Your service will make many things easier and I will now be able to order a larger number of pcbs. Ive finally had some time to redesign a board using SMT parts. Ive gone through the steps to get it ready for your service and have a few questions/comments about it.
The site seems pretty limited at the moment and didnt allow for uploading files or providing an estimated price. I assume this is because the database isnt online yet. I did what I could and what it would let me do worked fine although it was a little touchy about me staying logged in.
The tutorial and various scripts could do with some streamlining. Something similar to how BatchPCB has you run 1 script and the CAM job. Combining the various scripts together somehow and modifying the CAM job to include the .pads file would make things a little smoother at the beginning.
I am a little unclear about the multiple design thing. My intention was to design up 2 maybe 3 small pcbs (the current one is under 1" square with only 54 pads) and arrange them as I could in the space I could work with in Eagle (havnt 'gone pro' yet) so that the file I send to Gold Phoenix would have 3 of pcb1, 1 of pcb2 and 1 of pcb3. After sending it off to Gold Phoenix they would panelize the various pcbs so that in the end I would have a full panel of say 27 of pcb1, 9 of pcb2, and 9 of pcb3.
--While I would have 1 panel, it seems that for your service I would submit 3 different sets of files corresponding to each separate pcb. Is that correct or would I somehow have to send you the file for the whole panel?
--Does this incure additional cost or setup charges for the 3 different pcbs in the single panel?
--Under my rough estimate I would have about 45 total individual boards, each well under 200 pads... does that mean I get stuck with a $450 bill or is there some price range between a quantity of 10 and a quantity of 50 or would 45 boards be 'close enough' to 50 to count?
Finally I guess the big question is when do you plan to throw open the doors? I understand a lot of chips have to fall into place but is there any chance you might be going by this upcoming March?
Thank you so much and I look forward to giving your service a shot.
Brian Evans
Cal State Long Beach