- Thu May 17, 2007 3:46 pm
#30163
Hi all.
I'm new to eagle and this forum but not to board design in general.
I'm drawing up a board at the moment that needs thicker traces for the ac power nets. I created a class called ACPOWER and then changed the appropriate nets to use this class in the schematic. I then went back to the board, which I had already routed, ripped up the traces in question and then went to manually route them but they still default to the default trace settings. If I do an info on them it shows they have the appropriate class so why doesn't it route the wires with the new trace size I specified in the ACPOWER class?
If I pick the class before routing it seems to route with the right wire size. Does the manual router not automatically pick the trace width based on the class of the net being routed?
I'm new to eagle and this forum but not to board design in general.
I'm drawing up a board at the moment that needs thicker traces for the ac power nets. I created a class called ACPOWER and then changed the appropriate nets to use this class in the schematic. I then went back to the board, which I had already routed, ripped up the traces in question and then went to manually route them but they still default to the default trace settings. If I do an info on them it shows they have the appropriate class so why doesn't it route the wires with the new trace size I specified in the ACPOWER class?
If I pick the class before routing it seems to route with the right wire size. Does the manual router not automatically pick the trace width based on the class of the net being routed?