Analog & Digital GND on board but only 1 GND? how? PCM1803A

Questions relating to designing PCBs

Moderator: phalanx

Post Reply
alonper
Posts: 7
Joined: Thu Feb 08, 2018 10:40 am

Analog & Digital GND on board but only 1 GND? how? PCM1803A

Post by alonper » Thu Feb 08, 2018 11:06 am

Hi,

I will be glad to get some explanation about groud separation in PCBs,
I am looking at the design of the SparkFun PCM1803A (https://www.sparkfun.com/products/retired/9365)
and I see that in the schematic and in the PCB design, there are two grounds, Digital and Analog,
But there is only one source (+5v and GND) for the board, so how can it be?
why the grounds are separated on board and there is some small net bellow the PCM1803 chip that crosses the two grounds together?
Image

Thanks a lot!
best,
Alon

paulvha
Posts: 297
Joined: Sat Nov 11, 2017 2:39 am

Re: Analog & Digital GND on board but only 1 GND? how? PCM1803A

Post by paulvha » Fri Feb 09, 2018 10:45 am

The chip design seems to have had issues. From the data-sheet "To maximize the dynamic performance of the CM1803A, the analog and digital grounds are not connected internally. These grounds should have low impedance to avoid digital noise feeding back into the analog ground. Therefore, they should be connected directly to each other under the part to reduce potential noise problems."

alonper
Posts: 7
Joined: Thu Feb 08, 2018 10:40 am

Re: Analog & Digital GND on board but only 1 GND? how? PCM1803A

Post by alonper » Sat Feb 10, 2018 2:50 pm

So I don't really understand, there is ground separation, analog and digital, but they are the same ground so whats the point?
sorry if that a stupid question but I cant understand...
anyway if I would like to connect FMT and MD legs to the ground, Is it ok to connect to the "analog" ground?

paulvha
Posts: 297
Joined: Sat Nov 11, 2017 2:39 am

Re: Analog & Digital GND on board but only 1 GND? how? PCM1803A

Post by paulvha » Sun Feb 11, 2018 2:37 am

All depends on the chips and the circuit required. In some situations one would like to have a galvanic separation between the input from the computer and the output signals. This can be for safety reasons or to reduce interference. Take the AD5722, a DAC, it his logical and analog grounds. The chips internally is designed such that the input signal is galvanically separated from the output. (often an opto-coupler is used). They have done this so the logical input signal can be completely separated from the analog supply and output. If however you do not have a separation need and use only one power supply, then you connect the different grounds together, as they have done on the board and as such analog ground = digital ground and you can use it as the same.

Post Reply