- Thu Dec 31, 2015 5:44 pm
#186932
Hi All,
Is it possible to create a 'device' using a 'symbol' with 3 pins, and a 'package' with 4 terminals? The part I wish to create is a linear voltage regulator in a SOT223 package with an 'In', a 'Gnd', and two 'Out' pins (one of the leads, and the 'tab'). I know I can add another pin to my symbol and all will be good, but I'd prefer not to have to do it this way. When I 'Connect' the symbol pins to the package terminals, I obviously want the Out pin on the symbol connected to both Out terminals on the package!
John
Is it possible to create a 'device' using a 'symbol' with 3 pins, and a 'package' with 4 terminals? The part I wish to create is a linear voltage regulator in a SOT223 package with an 'In', a 'Gnd', and two 'Out' pins (one of the leads, and the 'tab'). I know I can add another pin to my symbol and all will be good, but I'd prefer not to have to do it this way. When I 'Connect' the symbol pins to the package terminals, I obviously want the Out pin on the symbol connected to both Out terminals on the package!
John