- Wed Nov 18, 2015 7:48 pm
#186018
Hello,
I've decided that I'd like to take the schematic and board design a user posted in PDF format and make it an Eagle file so I can modify it a bit. It has a PIC and I really have no experiences with PICs as of yet. I'd like to learn about them though in the future. Anyway, I created the schematic in Eagle and then routed the board in Eagle. When I run the checks on the schematic though, I get an error saying the PIC's VSS is connected to GND and the PIC's VDD is connected to +5V. If I add the symbol for VDD and VSS though, on the board, I cannot connect it to the +5V and GND nets. Is there away to connect those VSSs and VDDs to +5V and GND? Or can I just safely ignore the error? Thanks!
I've decided that I'd like to take the schematic and board design a user posted in PDF format and make it an Eagle file so I can modify it a bit. It has a PIC and I really have no experiences with PICs as of yet. I'd like to learn about them though in the future. Anyway, I created the schematic in Eagle and then routed the board in Eagle. When I run the checks on the schematic though, I get an error saying the PIC's VSS is connected to GND and the PIC's VDD is connected to +5V. If I add the symbol for VDD and VSS though, on the board, I cannot connect it to the +5V and GND nets. Is there away to connect those VSSs and VDDs to +5V and GND? Or can I just safely ignore the error? Thanks!