- Tue Nov 10, 2015 3:41 pm
#185787
RossWaddell wrote:Some questions:They are needed if you are going to thermally isolate the plane around a device (regulator in this case).
Why are 2 additional ground plane polygons needed if the board already has top and bottom layer ones over the whole board?
Why do the drawn polygons need to overlap the device's pins?I explained this in the vid. Since the regulator's screw mount is grounded internally, the thermal plane should be grounded as well. The easiest way is to have the plane overlap the ground pin so Eagle will create a connection to the ground pin. You don't have to do it this way. You can always make a connection with a trace from one of the vias to the ground pin.
Should Thermals be removed from the vias?Yes
------------------------------------------------------------------------------------------------------------------------------------------------------------
//codlink
Available for circuit and PCB design, just PM me!
//codlink
Available for circuit and PCB design, just PM me!