- Fri Mar 20, 2015 7:54 am
#180543
I have a simple question regarding creating a custom part in Ultiboard.
If I create a SMD 28 pin IC, I lay out the pads, and number then with Pin 1 in top left, Pin 14 at the bottom left, Pin 15 bottom right, and pin 28 top right.
If I create a 28 pin through hole DIP IC, do I number the pins the same? When I look at my through hole component in Ultiboard, am I looking at the top of the board? If so, do I need to place the pins on the bottom of the board? Or does Ultiboard base everything on where the component is actually located?
Thanks.
If I create a SMD 28 pin IC, I lay out the pads, and number then with Pin 1 in top left, Pin 14 at the bottom left, Pin 15 bottom right, and pin 28 top right.
If I create a 28 pin through hole DIP IC, do I number the pins the same? When I look at my through hole component in Ultiboard, am I looking at the top of the board? If so, do I need to place the pins on the bottom of the board? Or does Ultiboard base everything on where the component is actually located?
Thanks.