Hello everyone.
So, I've bread-boarded my design, and it works great with one potential problem... I've noticed that my 5V regulator gets very hot. So hot that I would get burned if I held my finger on it. This was a TO-220 package. The 3.3V (also TO-220) didn't feel hot at all. I've measured that my circuit draws about 185mA while up and running, and it draws about 250mA as inrush when starting up. I calculated that I'm burning about 2W of power over the 5V regulator with 12V input. I was going to use SOT-223 packages for the final PCB, but now I'm thinking that this isn't going to work.
I've looked in the datasheet for the LD1117 and did some checking on line, but I'm not really sure on how to calculate thermal resistance and things like that. Perhaps someone could explain this to me? The data sheet (
http://www.st.com/stonline/stappl/st/co ... 000544.pdf) lists that that SOT-223 part has a Rjc=15, but it doesn't list Rja. I'm a little confused with this, so please correct me if I'm wrong. I figured that at 2W, I'm raising the case temperature of the SOT-223 by 15*2=30 degC above ambient. Say the max ambient temp is 35 degC, then the max temp that the case would be is 30+35=65 degC which is lower than the maximum of 125 degC. This seems to indicate that I'll be ok, but then where does the junction-to-ambient come into play? For example, for the TO-220 at 2W, I calculate that the temp will rise ((50+5) * 2) = 110 degC above ambient. So if ambient is 35 degC, then I've exceeded the maximum operating temperature. I guess one question would be when do you use the Rjc and when do you use Rja.
I'd really appreciate any help with this.
Now, while looking all of this thermal information up, I came across some information saying that I should be using switching regulators instead of linear regulators. I guess that would eliminate the heat problem, correct? Should I use switching regulators? Which ones are the equivalent to the LD1117's? Will they still allow me to have the same input spec of 8-12VDC?
Now for a related question...
I originally sized my PTC at 500mA, but if the current actually goes to 500mA @ 12V input, then my regulator would surely burn up. If I keep the linear regulators, should I change my PTC to a lower value? Given that the operating current of the circuit is 185mA and the inrush is 250mA, what should the PTC be sized to? What if I change to switching regulators?
Sorry for the long post. I'm at least happy that my first PCB project worked correctly on the breadboard!
Thanks for the help!