- Fri Feb 03, 2012 5:05 am
#139200
thanks for all the help! I have definitely learnt a lot from this thread!
Philba wrote:ahh yes, thanks! I have already got the board in the production que. as the sparkfun tutorial suggests if that is a problem, I can always solder one on.evanrich wrote:Yes, you are right. I was looking at the internal trace limit when when I responded. But, the key point is he's in no danger of smoking his traces.Philba wrote:Not bad for a first attempt at hand routing.12 mil can handle more than that. depending on temperature rise allowance, it can handle ~1A. I've got 16mil traces, can handle 1.2A
(12 mil trace can handle half an amp so you are probably ok)
Also, you should google what a decoupling capacitor is for, so you know why you need them. In short, it helps smooth out the power coming into your IC. While it may run fine on a breadboard, and for your application it may not really matter, when you start getting into more sensitive circuits using micros, having a clean power supply is really important. The cap helps smooth the incoming power out.
As to decoupling, it's a good idea but he only has one digital IC run at a pretty low speed. I'd put one more in but I bet he never sees a glitch without it.
thanks for all the help! I have definitely learnt a lot from this thread!