- Sat Feb 06, 2010 7:20 pm
#92886
The DRC bot failed my board for violating the 8 mil trace width limit. My traces are all greater than 8 mils and the only thing highlighted in the picture I got in the email is a single pixel vertical line down the right edge of the board:
any ideas? There certainly arent any components or traces over there... The edge of the polygon is there but I tried moving it away and re uploading but it still failed.
Also definitely no errors on the bottom layer.
edit: heres the log for the top layer:
any ideas? There certainly arent any components or traces over there... The edge of the polygon is there but I tried moving it away and re uploading but it still failed.
Also definitely no errors on the bottom layer.
edit: heres the log for the top layer:
Code: Select all
unmatched 274X paramblock OFA0B0 - len 6
Macro Name = OC8
Macro Consuming 5,1,8,0,0,1.08239X$1,22.5 [2]
PUSH 1.000000
PUSH 8.000000
PUSH 0.000000
PUSH 0.000000
PUSH 1.082390
FETCH 1
MUL
PUSH 22.500000
PRIM 5
Parse_OK
Arg: 0.0600
Looking up macro OC8 [0x671160]
Beginning GCODE run
Ending GCODE run
Created 6397 polygons
Found 0 errors
Partitioning....
Grouping...
Distance testing
MergeCount: 6234
tests: 2075295
Board boundaries: Rect: [0.018100,0.021100] -> [2.774100,2.777100], w: 2.756000, h: 2.756000
Found 163 groups
lengthdb size 0
DRC space fail: [0x780870 0x783750] 0.000100 - 0.006900
DRC space fail: [0x780870 0x7915d0] 0.000100 - 0.006900
DRC space fail: [0x783750 0x780870] 0.000100 - 0.006900
DRC space fail: [0x784b50 0x784bf0] 0.000100 - 0.006900
DRC space fail: [0x784bf0 0x784b50] 0.000100 - 0.006900
DRC space fail: [0x784bf0 0x788ed0] 0.000100 - 0.006900
DRC space fail: [0x788ed0 0x784bf0] 0.000100 - 0.006900
DRC space fail: [0x7915d0 0x780870] 0.000100 - 0.006900