SparkFun Forums 

Where electronics enthusiasts find answers.

Discussions about processor boards have here!
User avatar
By VA3SU
#224345
I have a sparkfun nrf52832 breakout board that needs to have it's bootloader installed. I am using a Segger j-link to program the bootloader from sparkfun's gethub https://github.com/sparkfun/nRF52832_Breakout. I have tried both versions.

I am able to use the Segger j-link to flash the bootloader and the Segger J-Flash says that it is programmed (Using .hex file) but regardless of what I do the blue led doesn't flash as it should. I have erased the flash and tried several times. Each time it says it's programming was successful.

I am able to programmer using SES to flash leds etc no problem. The problem seems to be with the hex files supplied by Sparkfun. I don't think they are correct. I have noticed the the person who seems to have done the firmware is no longer with Sparkfun.

There are several people on this forum asking how to flash the nrf52832 with the bootloader and sparkfun hasn't helped anyone on this topic.

Kevin
User avatar
By TS-Chris
#224357
Hi Kevin.

We might have the wrong firmware files posted. Try these, they are the ones our production department uses to build this board.
nRF52832_PGM.zip
You do not have the required permissions to view the files attached to this post.
User avatar
By VA3SU
#224382
Hello Chris

Thanks for the zip file. Inside I found the four files below. I've tried them all with an erase flash in between with no luck. After flashing I have done the two button reset with no blue led flashing. Can you tell me which file is the firmware I should be loading, as I mentioned I tried them all but I expect it is the dfu file that is the bootloader.

Using ses I was able to test the function of the blue led and the button on pin 6. The reset button also works...

Regards,
Kevin

nrf52832_DEV_KIT_s132.hex
nRF52832_ST_Firmware_v21.ino.hex
s132_nrf52_2.0.0_softdevice.hex
sfe_nrf52832_dfu.hex
User avatar
By TS-Chris
#224423
It looks like we bootload these with Nordic's nRF52832 Hardware Development Kit, I don't know if that makes any difference but you might need that in order for things to run properly. Here's the commands we use in production to do the programming:
Code: Select all
nrfjprog -e -f nrf52
nrfjprog --program C:\Users\%username%\Desktop\nRF52832_PGM\s132_nrf52_2.0.0_softdevice.hex -f nrf52 --chiperase
nrfjprog --program C:\Users\%username%\Desktop\nRF52832_PGM\sfe_nrf52832_dfu.hex -f nrf52
nrfjprog --reset -f nrf52
The procedure might be different if you're using a different programmer though.
User avatar
By VA3SU
#224424
Thanks Chris

That was a big help. The procedure with a J-Link is first erase.

Program with the s132_nrf52_2.0.0_softdevice.hex file
Then program with the sfe_nrf52832_dfu.hex file

The blue led starts to time bomb right away.

Regards,
Kevin