- Sun Dec 04, 2022 8:26 pm
#237482
Could someone send me a link to a simple program that I can load on the SparkFun Thing Plus - ESP32 WROOM
to have it pass information between it and the Windows Remote Desktop application via wifi without going through a
cloud service? I want the ESP32 to create a menu on the RDP that a user can select a file to be transferred out using the ESP32's SPI interface to another device. Also can I write my programs in C#?. If so does it require specific libraries? Thanks.
to have it pass information between it and the Windows Remote Desktop application via wifi without going through a
cloud service? I want the ESP32 to create a menu on the RDP that a user can select a file to be transferred out using the ESP32's SPI interface to another device. Also can I write my programs in C#?. If so does it require specific libraries? Thanks.