SparkFun Forums 

Where electronics enthusiasts find answers.

Discussions about processor boards have here!
User avatar
By Bipman
#238708
Hi

I think this is a processor issue. I've got an artemis module and the Weather board and am trying to compile and upload the weather board test program. It compiles and uploads perfectly but when it runs I get :-
Code: Select all
MicroMod Weather Carrier Board Test



++ MbedOS Error Info ++
Error Status: 0x80FF0144 Code: 324 Module: 255
Error Message: Assertion failed: status == osOK
Location: 0x24EE9
File: mbed-os/rtos/source/ThisThread.cpp+225
Error Value: 0x0
Current Thread: main Id: 0x100048E0 Entry: 0x25EF1 StackSize: 0x1000 StackMem: 0x10006560 SP: 0x100074BC 
For more info, visit: https://mbed.com/s/error?error=0x80FF0144&tgt=SFE_ARTEMIS_MM_PB
-- MbedOS Error Info --
I went to the link but it says the error is unknown. The light on the Artemis board flashes 4 times and then 5 fast flashes and then goes round again. Any ideas?

Bipman
User avatar
By Bipman
#238709
It's something to do with the test program as below because the sensor programmes on their own work fine.
Code: Select all
/*
 * MicroMod Weather Carrier Board Example
 * 
 * This sketch tests all of the weather sensors on the carrier board:
 * atmospheric sensor - BME280, UV sensor - VEML6075, lightning detector - AS3935,
 * soil moisture sensor, wind and rain meters.
 * 
 * Priyanka Makin @ SparkX Labs
 * Original Creation Date: August 20, 2020
 * 
 * This code is Lemonadeware; if you see me (or any other SparkFun employee) at the
 * local, and you've found our code helpful, please buy us a round!
 * 
 * Hardware Connections:
 * Insert MicroMod Processor Board of your choice into the M.2 connector of the SparkFun Weather carrier
 *  Screw into place
 * Connect Weather carrier board to power useing USB-C cable
 * Connect SparkFun Soil Moisture Sensor to Weather carrier using latching terminals
 * Connect both wind and rain meters to Weather carrier using the RJ11 connectors
 */

#include <Wire.h>
#include <SPI.h>
#include "SparkFunBME280.h"
#include <SparkFun_VEML6075_Arduino_Library.h>
#include "SparkFun_AS3935.h"

BME280 tempSensor;
VEML6075 uv;
SparkFun_AS3935 lightning;

#define INDOOR 0x12 
#define OUTDOOR 0xE
#define LIGHTNING_INT 0x08
#define DISTURBER_INT 0x04
#define NOISE_INT 0x01

#if defined(ESP_PLATFORM)
int LED_BUILTIN = 5;
//int A0 = 34;
int G0 = 4;
int D0 = 23;
//int A1 = 35;
int D1 = 27;
const int G3 = 17;
int G1 = 12;
#elif defined(ARDUINO_ARCH_SAMD)
int G0 = 2;
int D0 = 0;
int D1 = 1;
//const int lightningInt = G3;  //SPI does not currently work on the SAMD51 proto
//int spiCS = G1;
#endif

int soilPin = A0;  //Pin number that measures analog moisture signal
int soilPower = G0;  //Pin number that will power the soil moisture sensor
int WSPEED = D0; //Digital I/O pin for wind speed
int WDIR = A1; //Analog pin for wind direction
int RAIN = D1;   //Digital I/O pin for rain fall
const int lightningInt = G3; // Interrupt pin for lightning detection
int spiCS = G1; //SPI chip select pin

volatile bool rainFlag = false;
volatile bool windFlag = false;

//Function is called every time the rain bucket tips
void rainIRQ()
{
  rainFlag = true;
}

//Function is called when the magnet in the anemometer is activated
void wspeedIRQ()
{
  windFlag = true;
}

// This variable holds the number representing the lightning or non-lightning
// event issued by the lightning detector. 
int intVal = 0;
int noise = 2; // Value between 1-7 
int disturber = 2; // Value between 1-10

void setup() {
  Serial.begin(115200);
  while (!Serial);

  Serial.println("MicroMod Weather Carrier Board Test");
  Serial.println();

  Wire.begin();
  SPI.begin();

  if (tempSensor.beginI2C() == false) { //Begin communication over I2C
    Serial.println("BME280 did not respond.");
    while(1); //Freeze
  }
  if (uv.begin() == false) {
    Serial.println("VEML6075 did not respond.");
    while(1);
  }

  pinMode(LED_BUILTIN, OUTPUT);
  pinMode(soilPower, OUTPUT);
  digitalWrite(soilPower, LOW);
  // When lightning is detected the interrupt pin goes HIGH.
  pinMode(lightningInt, INPUT);

  //Initialization for weather meter
  pinMode(WSPEED, INPUT_PULLUP);  //Input from wind meters windspeed sensor
  pinMode(RAIN, INPUT_PULLUP);    //Input from wind meters rain gauge sensor
  //attach external interrupt pins to IRQ functions
  attachInterrupt(digitalPinToInterrupt(RAIN), rainIRQ, FALLING);
  attachInterrupt(digitalPinToInterrupt(WSPEED), wspeedIRQ, FALLING);
  //turn on interrupts
  interrupts();

  if(lightning.beginSPI(spiCS, 2000000) == false){ 
    Serial.println ("Lightning Detector did not start up, freezing!"); 
    while(1); 
  }
  else
    Serial.println("Schmow-ZoW, Lightning Detector Ready!");

  // The lightning detector defaults to an indoor setting at 
  // the cost of less sensitivity, if you plan on using this outdoors 
  // uncomment the following line:
  lightning.setIndoorOutdoor(OUTDOOR); 
}

// the loop function runs over and over again forever
void loop() {
  digitalWrite(LED_BUILTIN, HIGH);   // turn the LED on (HIGH is the voltage level)

  Serial.println();
  Serial.print("Temperature: ");
  Serial.println(tempSensor.readTempF(), 2);
  Serial.print("Humidity: ");
  Serial.println(tempSensor.readFloatHumidity(), 0);
  Serial.print("Pressure: ");
  Serial.println(tempSensor.readFloatPressure(), 0);
  Serial.print("Altitude: ");
  Serial.println(tempSensor.readFloatAltitudeFeet(), 1);

  Serial.print("UV A, B, index: ");
  Serial.println(String(uv.uva()) + ", " + String(uv.uvb()) + ", "+ String(uv.index()));

  Serial.print("Soil Moisture = ");
  Serial.println(readSoil());

  Serial.print("Wind direction: ");
  Serial.print(getWindDirection());
  Serial.println(" degrees");
  //Check interrupt flags
  if (rainFlag == true){
    Serial.println("Rain click!");
    rainFlag = false;
  }
  if (windFlag == true){
    Serial.println("Wind click!");
    windFlag = false;
  }

  // Hardware has alerted us to an event, now we read the interrupt register
  if(digitalRead(lightningInt) == HIGH){
    intVal = lightning.readInterruptReg();
    if(intVal == NOISE_INT){
      Serial.println("Noise."); 
      // Too much noise? Uncomment the code below, a higher number means better
      // noise rejection.
      //lightning.setNoiseLevel(noise); 
    }
    else if(intVal == DISTURBER_INT){
      Serial.println("Disturber."); 
      // Too many disturbers? Uncomment the code below, a higher number means better
      // disturber rejection.
      //lightning.watchdogThreshold(disturber);  
    }
    else if(intVal == LIGHTNING_INT){
      Serial.println("Lightning Strike Detected!"); 
      // Lightning! Now how far away is it? Distance estimation takes into
      // account any previously seen events in the last 15 seconds. 
      byte distance = lightning.distanceToStorm(); 
      Serial.print("Approximately: "); 
      Serial.print(distance); 
      Serial.println("km away!"); 
    }
  }

  digitalWrite(LED_BUILTIN, LOW);    // turn the LED off by making the voltage LOW

  delay(3000);
}

int readSoil() {
  int moistVal = 0;  //Variable for storing moisture value
  //Power Senor
  digitalWrite(soilPower, HIGH);
  delay(10);
  moistVal = analogRead(soilPin);  //Read the SIG value from sensor
  digitalWrite(soilPower, LOW); //Turn the sensor off
  return moistVal; //Return current moisture value
}

int getWindDirection()
{
  unsigned int adc;
  adc = analogRead(WDIR); //get the current readings from the sensor

  if (adc < 380) return (113);
  if (adc < 393) return (68);
  if (adc < 414) return (90);
  if (adc < 456) return (158);
  if (adc < 508) return (135);
  if (adc < 551) return (203);
  if (adc < 615) return (180);
  if (adc < 680) return (23);
  if (adc < 746) return (45);
  if (adc < 801) return (248);
  if (adc < 833) return (225);
  if (adc < 878) return (338);
  if (adc < 913) return (0);
  if (adc < 940) return (293);
  if (adc < 967) return (315);
  if (adc < 990) return (270);
  return (-1);
}
Bipman
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum

long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]