Error flashing an PCI-based FPGA card (PCIeScreamer)

Open source ARM Debugger

Moderator: phalanx

Post Reply
CuriosoCat
Posts: 1
Joined: Thu Jan 03, 2019 8:08 pm

Error flashing an PCI-based FPGA card (PCIeScreamer)

Post by CuriosoCat » Thu Jan 03, 2019 8:26 pm

Hi all,

So i'm experiencing an error while using openocd to flash my bitstream into an FPGA device (PCIeScreamer) as seen below. I've logged this issue on the relevant github page and tried several solutions to no avail. I'm wondering if anyone experienced enough can help me identify if this is an openocd issue. Any help would be greatly appreciated!

Code: Select all

$ sudo openocd -f flash_screamer.cfg
Open On-Chip Debugger 0.10.0+dev-00631-ga15c11d (2018-12-26-14:04)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
none separate
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
adapter speed: 10000 kHz
Info : ftdi: if you experience problems at higher adapter clocks, try the command "ftdi_tdo_sample_edge falling"
Info : clock speed 10000 kHz
Info : JTAG tap: xc7.tap tap/device found: 0x0362d093 (mfg: 0x049 (Xilinx), part: 0x362d, ver: 0x0)
loaded file bscan_spi_xc7a35t.bit to pld device 0 in 0s 219832us
Info : JTAG tap: xc7.tap tap/device found: 0x0362d093 (mfg: 0x049 (Xilinx), part: 0x362d, ver: 0x0)
Info : Found flash device 'micron n25q256 3v' (ID 0x0019ba20)
Warn : device needs paging or 4-byte addresses - not implemented
flash 'jtagspi' found at 0x00000000
auto erase enabled
Info : Found flash device 'micron n25q256 3v' (ID 0x0019ba20)
Warn : device needs paging or 4-byte addresses - not implemented
Info : Found flash device 'micron n25q256 3v' (ID 0x0019ba20)
Warn : device needs paging or 4-byte addresses - not implemented
Info : Found flash device 'micron n25q256 3v' (ID 0x0019ba20)
Warn : device needs paging or 4-byte addresses - not implemented
Info : sector 0 took 0 ms
Info : sector 1 took 0 ms
Info : sector 2 took 0 ms
Info : sector 3 took 1 ms
Info : sector 4 took 0 ms
Info : sector 5 took 0 ms
Info : sector 6 took 0 ms
Info : sector 7 took 1 ms
Info : sector 8 took 0 ms
Info : sector 9 took 0 ms
Info : sector 10 took 0 ms
Info : sector 11 took 1 ms
Info : sector 12 took 0 ms
Info : sector 13 took 0 ms
Info : sector 14 took 0 ms
Info : sector 15 took 1 ms
Info : sector 16 took 0 ms
Info : sector 17 took 0 ms
Info : sector 18 took 0 ms
Info : sector 19 took 1 ms
Info : sector 20 took 0 ms
Info : sector 21 took 0 ms
Info : sector 22 took 0 ms
Info : sector 23 took 1 ms
wrote 1572864 bytes from file pcileech_pciescreamer_top.bin in 9.611363s (159.811 KiB/s)
Info : Found flash device 'micron n25q256 3v' (ID 0x0019ba20)
Warn : device needs paging or 4-byte addresses - not implemented
read 1512368 bytes from file pcileech_pciescreamer_top.bin and flash bank 0 at offset 0x00000000 in 1.291909s (1143.209 KiB/s)
contents differ
diff 0 address 0x00000085. Was 0x10 instead of 0x30
diff 1 address 0x0000009f. Was 0x01 instead of 0x13
diff 2 address 0x000000a0. Was 0x20 instead of 0x30
diff 3 address 0x000000a2. Was 0x00 instead of 0x80
diff 4 address 0x000000a3. Was 0x00 instead of 0x01
diff 5 address 0x000000a7. Was 0x01 instead of 0x09
diff 6 address 0x000000a8. Was 0x00 instead of 0x20
diff 7 address 0x000000ae. Was 0x80 instead of 0xc0
diff 8 address 0x000000b6. Was 0x80 instead of 0xa0
diff 9 address 0x000000ba. Was 0x00 instead of 0x05
diff 10 address 0x000000bb. Was 0x00 instead of 0x01
diff 11 address 0x000000be. Was 0x00 instead of 0xc0
diff 12 address 0x000000c2. Was 0x00 instead of 0x10
diff 13 address 0x000000c4. Was 0x20 instead of 0x30
diff 14 address 0x000000c5. Was 0x00 instead of 0x03
diff 15 address 0x000000c7. Was 0x00 instead of 0x01
diff 16 address 0x000000ca. Was 0x00 instead of 0x10
diff 17 address 0x000000e8. Was 0x00 instead of 0x20
diff 18 address 0x000000ee. Was 0x00 instead of 0x20
diff 19 address 0x000000f4. Was 0x20 instead of 0x30
diff 20 address 0x000000f6. Was 0x00 instead of 0x80
diff 21 address 0x000000f7. Was 0x00 instead of 0x01
diff 22 address 0x000000fb. Was 0x00 instead of 0x01
diff 23 address 0x000000fc. Was 0x00 instead of 0x20
diff 24 address 0x00000100. Was 0x00 instead of 0x30
diff 25 address 0x00000102. Was 0x00 instead of 0x41
diff 26 address 0x00000103. Was 0x00 instead of 0x94
diff 27 address 0x0000011b. Was 0x00 instead of 0x84
diff 28 address 0x00000127. Was 0x00 instead of 0x0a
diff 29 address 0x000001be. Was 0x00 instead of 0x08
diff 30 address 0x000001c3. Was 0x00 instead of 0x88
diff 31 address 0x000001c6. Was 0x00 instead of 0x08
diff 32 address 0x000001cb. Was 0x00 instead of 0x88
diff 33 address 0x000001cf. Was 0x00 instead of 0x47
diff 34 address 0x00000352. Was 0x00 instead of 0x40
diff 35 address 0x00000357. Was 0x00 instead of 0x60
diff 36 address 0x0000035a. Was 0x00 instead of 0x40
diff 37 address 0x0000035f. Was 0x00 instead of 0x60
diff 38 address 0x00000362. Was 0x00 instead of 0x10
diff 39 address 0x00000363. Was 0x00 instead of 0x40
diff 40 address 0x000004f6. Was 0x00 instead of 0x15
diff 41 address 0x000004f7. Was 0x00 instead of 0x7c
diff 42 address 0x00000534. Was 0x00 instead of 0x08
diff 43 address 0x0000054b. Was 0x00 instead of 0x80
diff 44 address 0x0000057b. Was 0x00 instead of 0x40
diff 45 address 0x000005ab. Was 0x00 instead of 0x40
diff 46 address 0x00000754. Was 0x00 instead of 0x30
diff 47 address 0x00000756. Was 0x00 instead of 0x80
diff 48 address 0x00000757. Was 0x00 instead of 0x01
diff 49 address 0x0000075b. Was 0x00 instead of 0x02
diff 50 address 0x0000075c. Was 0x00 instead of 0x20
diff 51 address 0x00000760. Was 0x00 instead of 0x20
diff 52 address 0x00000764. Was 0x00 instead of 0x20
diff 53 address 0x00000768. Was 0x00 instead of 0x20
diff 54 address 0x0000076c. Was 0x00 instead of 0x20
diff 55 address 0x00000770. Was 0x00 instead of 0x20
diff 56 address 0x00000774. Was 0x00 instead of 0x20
diff 57 address 0x00000778. Was 0x00 instead of 0x20
diff 58 address 0x0000077c. Was 0x00 instead of 0x20
diff 59 address 0x00000780. Was 0x00 instead of 0x20
diff 60 address 0x00000784. Was 0x00 instead of 0x20
diff 61 address 0x00000788. Was 0x00 instead of 0x20
diff 62 address 0x0000078c. Was 0x00 instead of 0x30
diff 63 address 0x0000078d. Was 0x00 instead of 0x01
diff 64 address 0x0000078e. Was 0x00 instead of 0x40
diff 65 address 0x0000078f. Was 0x00 instead of 0x08
diff 66 address 0x000007b0. Was 0x00 instead of 0x30
diff 67 address 0x000007b2. Was 0x00 instead of 0x20
diff 68 address 0x000007b3. Was 0x00 instead of 0x01
diff 69 address 0x000007b7. Was 0x00 instead of 0x08
diff 70 address 0x000007b8. Was 0x00 instead of 0x30
diff 71 address 0x000007b9. Was 0x00 instead of 0x01
diff 72 address 0x000007ba. Was 0x00 instead of 0x40
diff 73 address 0x000007bb. Was 0x00 instead of 0x04
diff 74 address 0x000007cc. Was 0x00 instead of 0x30
diff 75 address 0x000007ce. Was 0x00 instead of 0x20
diff 76 address 0x000007cf. Was 0x00 instead of 0x01
diff 77 address 0x000007d3. Was 0x00 instead of 0x0a
diff 78 address 0x000007d4. Was 0x00 instead of 0x30
diff 79 address 0x000007d5. Was 0x00 instead of 0x01
diff 80 address 0x000007d6. Was 0x00 instead of 0x40
diff 81 address 0x000007d7. Was 0x00 instead of 0x04
diff 82 address 0x000007e8. Was 0x00 instead of 0x30
diff 83 address 0x000007ea. Was 0x00 instead of 0x20
diff 84 address 0x000007eb. Was 0x00 instead of 0x01
diff 85 address 0x000007ef. Was 0x00 instead of 0x14
diff 86 address 0x000007f0. Was 0x00 instead of 0x30
diff 87 address 0x000007f1. Was 0x00 instead of 0x01
diff 88 address 0x000007f2. Was 0x00 instead of 0x40
diff 89 address 0x000007f3. Was 0x00 instead of 0x04
diff 90 address 0x00000804. Was 0x00 instead of 0x30
diff 91 address 0x00000806. Was 0x00 instead of 0x20
diff 92 address 0x00000807. Was 0x00 instead of 0x01
diff 93 address 0x0000080b. Was 0x00 instead of 0x1a
diff 94 address 0x0000080c. Was 0x00 instead of 0x30
diff 95 address 0x0000080d. Was 0x00 instead of 0x01
diff 96 address 0x0000080e. Was 0x00 instead of 0x40
diff 97 address 0x0000080f. Was 0x00 instead of 0x04
diff 98 address 0x00000820. Was 0x00 instead of 0x30
diff 99 address 0x00000822. Was 0x00 instead of 0x20
diff 100 address 0x00000823. Was 0x00 instead of 0x01
diff 101 address 0x00000827. Was 0x00 instead of 0x1b
diff 102 address 0x00000828. Was 0x00 instead of 0x30
diff 103 address 0x00000829. Was 0x00 instead of 0x01
diff 104 address 0x0000082a. Was 0x00 instead of 0x40
diff 105 address 0x0000082b. Was 0x00 instead of 0x04
diff 106 address 0x0000083c. Was 0x00 instead of 0x30
diff 107 address 0x0000083e. Was 0x00 instead of 0x20
diff 108 address 0x0000083f. Was 0x00 instead of 0x01
diff 109 address 0x00000843. Was 0x00 instead of 0x22
diff 110 address 0x00000844. Was 0x00 instead of 0x30
diff 111 address 0x00000845. Was 0x00 instead of 0x01
diff 112 address 0x00000846. Was 0x00 instead of 0x40
diff 113 address 0x00000847. Was 0x00 instead of 0x04
diff 114 address 0x00000858. Was 0x00 instead of 0x30
diff 115 address 0x0000085a. Was 0x00 instead of 0x20
diff 116 address 0x0000085b. Was 0x00 instead of 0x01
diff 117 address 0x0000085f. Was 0x00 instead of 0x23
diff 118 address 0x00000860. Was 0x00 instead of 0x30
diff 119 address 0x00000861. Was 0x00 instead of 0x01
diff 120 address 0x00000862. Was 0x00 instead of 0x40
diff 121 address 0x00000863. Was 0x00 instead of 0x04
diff 122 address 0x00000874. Was 0x00 instead of 0x30
diff 123 address 0x00000876. Was 0x00 instead of 0x20
diff 124 address 0x00000877. Was 0x00 instead of 0x01
diff 125 address 0x0000087b. Was 0x00 instead of 0x24
diff 126 address 0x0000087c. Was 0x00 instead of 0x30
diff 127 address 0x0000087d. Was 0x00 instead of 0x01
More than 128 errors, the rest are not printed.

Post Reply