- Mon Oct 22, 2018 9:12 am
#200740
Quick question before I try a FT2232H chip and make sure I'm not doing something incorrectly. Here is the output when doing a sysview trace using a J-Link EDU. Would SEGGER's licensing cause the failure? GDB works fine, but trace does not.
Code: Select all
> esp32 sysview start file://pro-cpu.SVDat file://app-cpu.SVDat
Target halted. PRO_CPU: PC=0x400E23A2 (active) APP_CPU: PC=0x00000000
Total trace memory: 16384 bytes
Open file pro-cpu.SVDat
Open file app-cpu.SVDat
App trace params: from 2 cores, size 4294967295 bytes, stop_tmo -1 s, poll period 1 ms, wait_rst 0, skip 0 bytes
Connect targets...
Target halted. PRO_CPU: PC=0x400E23A2 (active) APP_CPU: PC=0x00000000
Targets connected.
Stop waiting for trace start due to timeout.
SEGGER: Failed to start tracing!
Disconnect targets...
Target halted. PRO_CPU: PC=0x400E23A2 (active) APP_CPU: PC=0x00000000
Targets disconnected.
Trace data processor thread exited with 0