JTAG-DP STICKY ERROR - Photon

Open source ARM Debugger

Moderator: phalanx

Post Reply
JohnKoz
Posts: 6
Joined: Mon Feb 06, 2017 4:24 pm

JTAG-DP STICKY ERROR - Photon

Post by JohnKoz » Mon Dec 11, 2017 5:35 am

Hi folks,

I've searched quite a bit regarding the error I'm seeing in OpenOCD, when connecting to the Particle Programmer Shield and the Photon. I haven't been able to get past this for weeks.

Are there any tips or hints on how to troubleshoot this error? Even narrowing it down between firmware build, hardware error, configuration, etc. would help.

I attach an ARM GDB debugger to port 3333 on OpenOCD for remote debugging. In the simplest case, whenever I try to examine memory, I receive a JTAG-DP STICKY ERROR. I can examine registers fine, continue execution, etc.

Code: Select all

openocd -f particle-ftdi.cfg -f stm32f2x.cfg -c "gdb_port 3333"
For example, if I issue:
x 0x08068b32
I'll see the following error on the OpenOCD console.
Error: JTAG-DP STICKY ERROR
Error: Failed to read memory at 0x08068b32
And I'll get back zero's for memory content in the debugger.

Any idea? Where could I look? I've tried different adapter speeds (ex: 500, 1000, 10000).

Thanks!

-John

Post Reply